Link RBI Corrosion Loops to a Unit

Steps

  1. Access the Risk Based Inspection Overview page for the unit to which you want to link RBI Corrosion Loops.
  2. In the workspace heading, select the Corrosion Loops tab.

    The Corrosion Loops section appears, displaying a list of RBI Corrosion Loops contained in the unit.

    Note: You can link RBI Corrosion Loops only to units that have the Is a Process Unit? check box selected in Record Manager.

  3. In the upper-right corner of the section, select .

    The Select Corrosion Loops window appears.

  4. Next to the RBI Corrosion Loops that you want to link to the unit, select the check boxes, and then select Done.

    The selected RBI Corrosion Loops are linked to the unit.