Allowable Stress

When you create an RBI Analysis , several values are copied automatically to fields in the RBI Analysis. Along with the following values, these copied values are used to determine the value that appears by default in the Allowable Stress field in that RBI Analysis:

The following steps list the process to determine the value in the Allowable Stress field:

  1. You create an RBI Analysis, which copies values from the associated RBI Components to the RBI Analysis.
  2. Meridium Enterprise APM looks for values in the Stress Lookup Table field in the associated RBI Component.
  3. Depending on the values in the Stress Lookup Table field, Meridium Enterprise APM looks for values in a specific reference table.
  4. The Meridium Enterprise APM system maps various values in the RBI Analysis (which were copied in step 1) to the values in the reference table to find the correct value with which to populate the Allowable Stress field in the RBI Analysis.