RBI Strategy Mapping Configuration

The RBI Strategy Mapping Configuration family defines the Policy records that are used to generate RBI Recommendation records automatically from RBI Analyses. The information in the table reflects the baseline state and behavior of fields that exist in the RBI Strategy Mapping Configuration family.

RBI Strategy Mapping Configuration Details

Field Data Type Description Behavior and Usage
Degradation Mechanism Character The value in the Degradation Mechanism field linked to the RBI Analysis for which you are generating RBI Recommendations. This field is populated by default in each RBI Strategy Mapping Configuration that is delivered to the baseline Meridium Enterprise APM database.
Policy Name Character The Record ID of the Policy used to generate an RBI Recommendation. This field is populated by default in each RBI Strategy Mapping Configuration that is delivered to the baseline Meridium Enterprise APM database.

RBI Strategy Mapping Details define the Policy Input nodes that are used to generate RBI Recommendation records automatically from RBI Analyses. The information in the table reflects the baseline state and behavior of fields in the RBI Strategy Mapping Details family.

RBI Strategy Mapping Details

Field Data Type Description Behavior and Usage
Policy Input Node Name Character The ID of the Input node in the Policy that is defined by the RBI Strategy Mapping Configuration to which the RBI Strategy Mapping Details is linked. This field is populated by default in each RBI Policy that is delivered to the baseline Meridium Enterprise APM database.
Source Family Character The family of the source record whose values are used to determine the output of the Input node. This field is populated by default in each RBI Strategy Mapping Details that is delivered to the baseline Meridium Enterprise APM database.
Source Field Character The field whose source value is used to determine the output of the Input node. This field is populated by default in each RBI Strategy Mapping Details that is delivered to the baseline Meridium Enterprise APM database.