System Code Tables Used by Risk Based Inspection

RBI 580

The following table lists the System Code Tables that are used by RBI 580.

Table ID Table Description Function

MI DAMAGE FACTOR

Damage Factor Class

The values in this System Code Table are used when you calculate an RBI PRD Analysis.

MI_DEGRADATION_MECHANISM_TYPES

Degradation Mechanism Types

Populates the Degradation Mechanism list in Potential Degradation Mechanism records.

MI GROUPING CORR TYPE

Grouping Corrosion Types

Populates the Corrosion Type list.

MI GROUPING EQP TYPE

Grouping Equipment Types

Populates the Grouping Equipment Type list.

MI INSPECTION RESULT

Inspection Result

Populates the Test Results list in Criticality Over Pressure Deg. Mech. Eval. and Criticality Leak Deg. Mech. Eval. records.

MI PDM FILTER

MI RBI, Potential Degradation Filter

Used to limit the Potential Degradation Mechanisms records that can be linked to RBI Components.

MI PRD DISCHARGE LOCATION

MI PRD DISCHARGE LOCATION

Populates the PRD Discharge Location list in RBI PRD Criticality Analysis records.

MI PROTECTED EQUIP TYPES

Protected Equipment Types

Populates the Protected Equipment Type list in RBI PRD Criticality Analysis records.

MI RBI RISK CATEGORY

RBI Risk Category

Populates the Risk Categorylist in Asset Group records.

MI SERVICE SEVERITY

Severity of the Process Fluid

Populates the Service Severity list in RBI PRD Criticality Analysis records.

Pipeline Management

The following table lists the System Code Tables that are used by Pipeline Management

Table ID Table Description Function

MI PIPELINEBELOWWATERSURFACE

Depth Below Water Surface

The values in this table are used to populate the list in the Below Water Surface field in Criticality Third Party Deg. Mech. Eval. records.

MI PIPELINEPROTECTIONCOVER Mechanical Pipe Protection The values in this table are used to populate the list in the Mechanical Pipe Protection field in Criticality Third Party Deg. Mech. Eval. records.
MI PIPELINEWARNINGSTRIP Warning Strip The values in this table are used to populate the list in the Pipeline Marker Tape field in Criticality Third Party Deg. Mech. Eval. records.
MI PIPELINEBELOWBOTTOMWATERWAY Depth Below Bottom of Waterway The values in this table are used to populate the list in the Below Bottom of Waterway field in Criticality Third Party Deg. Mech. Eval. records.
MI PIPELINECONCRETECOATING Concrete Coating The values in this table are used to populate the list in the Concrete Coating field in Criticality Third Party Deg. Mech. Eval. records.
MI PIPELINEACTIVITYLEVEL Activity Level The values in this table are used to populate the list in the Activity Level field in Criticality Third Party Deg. Mech. Eval. records.
MI PIPELINEABOVEGROUNDFACILITY Above Ground Facilities The values in this table are used to populate the list in the Above Ground Facilities field in Criticality Third Party Deg. Mech. Eval. records.
MI PIPELINELINELOCATING Line Locating (One-Call System) The values in this table are used to populate the list in the One-Call System field in Criticality Third Party Deg. Mech. Eval. records.
MI PIPELINEEDUCATIONPROGRAM Public Education Program The values in this table are used to populate the list in the Public Education field in Criticality Third Party Deg. Mech. Eval. records.
MI PIPELINERIGHTOFWAY Right-Of-Way Condition The values in this table are used to populate the list in the Right-Of-Way Condition field in Criticality Third Party Deg. Mech. Eval. records.
MI PIPELINEPATROLFREQ Patrol Frequency The values in this table are used to populate the list in the Patrol Frequency field in Criticality Third Party Deg. Mech. Eval. records.
MI PIPELINEPREVIOUSDAMAGE Previous Damage The values in this table are used to populate the list in the Previous Damage field in Criticality Third Party Deg. Mech. Eval. records.
MI PIPELINELANDMOVEMENTPOTENTIAL Land Movement Potential The values in this table are used to populate the list in the the RBI Pipeline Analysis and Criticality RBI Pipeline Segment families.
MI PIPELINEPRESSURESURGEPOTENTIAL Pressure Surge Potential The values in this System Code Table are used by the RBI Pipeline Analysis and Criticality RBI Pipeline Segment families.
MI PIPELINESCADA SCADA Level The values in this table are used to populate the list in the SCADA field in the RBI Pipeline Analysis and Criticality RBI Pipeline Segment families.
MI PIPELINEPOPULATIONDENSITYADJUSTED Population Density Adjustment The values in this System Code Table are used to populate the list in the Population Density field in Pipeline Consequence Evaluation records.
MI PIPELINESOILTYPEFACTOR Soil Type Factor The values in this System Code Table are used to populate the list in the Soil Type field in Pipeline Consequence Evaluation records.
MI PIPELINEHIGHVALUEAREAFACTOR High Value Area Factor The values in this System Code Table are used to populate the list in the High Value Area field in Pipeline Consequence Evaluation records.
MI PIPELINESUGGESTEDCLEANUPCOSTS Suggested Clean Up Costs The values in this System Code Table are used to populate the list in the Suggested Clean Up field in Pipeline Consequence Evaluation records.
MI PIPELINE SEGMENT TYPE Segment Type The values in this System Code Table are used to populate the list in the Segment Type field in RBI Pipeline Segment records.