Unlink RBI Corrosion Loops from a Unit

Steps

  1. Access the Risk Based Inspection Overview page for the unit from which you want to unlink RBI Corrosion Loops.
  2. In the workspace heading, select the Corrosion Loops tab.

    The Corrosion Loops section appears, displaying a list of RBI Corrosion Loops contained in the unit.

  3. In the upper-right corner of the section, select .

    The Select Corrosion Loops window appears.

  4. Next to the RBI Corrosion Loops that you want to unlink from the unit, select the check boxes, and then select Done.

    The selected RBI Corrosion Loops are linked to the unit.