Create Custom Degradation Mechanism Evaluation (DME) Validation Policies

Steps

  1. Create a new policy to validate your custom DME.

  2. Select .
  3. On the Policy Designer page, in the left pane, select Design.

    The Design workspace appears.

  4. On the workspace heading, in the Inputs section, select, and then select Entity.

    A new Entity node appears in the Design workspace.

  5. Select the new Entity node, and then, in the Properties box, in the Family ID field, select the family of the custom DME you are validating

    Note: Repeat steps 4 and 5 to add any other entity nodes required for validations, such as Analysis validations, Consequence Evaluation validations, or validations for other DMEs that are related to the same analysis.
  1. Using the Input Entity nodes, perform all required validations.

  2. Select .

    The custom DME validation policy is saved.