Steps
In the lower-left corner of the workspace, select the Hypothesis List pane.
A list of Hypotheses available in the database for the selected RCA appears.
Note: If any RCA Hypothesis are linked to the current RCA but do not appear in the Logic Tree, they will appear in the list.
Select the row containing the Hypothesis that you want to add.
In the upper-right corner of the pane, select Add to Selected Node.
The new Hypothesis node appears on the Logic Tree at the specified location .
Note: As needed, you can modify the Hypothesis node. To do so, select the Hypothesis, and then select
Copyright © 1993-2016 Meridium, Inc. All rights reserved.