Overview of Root Cause Analysis Module

The Meridium Enterprise APM Root Cause Analysis (RCA) module lets you conduct a root cause analysis, which allows you to analyze causes of failures. A root cause analysis also allows you to track the performance of the equipment by following implementation of recommendations. When you create a Root Cause analysis, you are using Meridium Enterprise APM tools to facilitate a standard process that is based on the PROACT® for Meridium methodology.

Note: The RCA module is based on the PROACT® RCA Methodology, © Copyright 1996 - 2015, RCI-Reliability Center Incorporated. All rights reserved. Used with Permission.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.