About PROACT for Meridium

PROACT for Meridium is a methodology that is used in the RCA module that allows you to conduct a root cause analysis.

The PROACT acronym consists of the following steps, where the letters that make up the acronym are capitalized:

You can use these steps as a guideline for conducting a Root Cause Analysis in the RCA module, which consists of creating the data in Meridium Enterprise APM that is necessary to complete these five steps of the PROACT for Meridium methodology and implement successful solutions.

Note: You are not required to complete these steps in the exact order that they are listed above. It is important, however, that all steps of the methodology be completed. For more information, see the workflow for conducting a Root Cause Analysis.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.