The Meridium Enterprise APM system automatically arranges the presentation of the nodes of the Logic Tree diagram in the design canvas. You can accept this default setting and allow Meridium Enterprise APM system to control the display of the Logic Tree, or you can disable this feature and manually rearrange the location of the nodes. If you choose to manually arrange nodes, the arrangements are not saved. When you open the diagram again, it will be auto-arranged.
Steps
In the upper portion of the workspace, select
In the design canvas, select and drag the required node to the required location in the Logic Tree.
Note: If you disable the Auto Arrange option, manually change the location of the nodes, and then reselect the Auto Arrange option, the system will over-ride all of the manual changes and apply the system defaults to the Logic Tree.
Copyright © 1993-2016 Meridium, Inc. All rights reserved.