The Cause Report displays information that is stored in RCA Hypothesis records that are linked to the RCA Analysis record and contain a value of Cause - Physical, Cause - Latent, or Cause - Human in the State field. This information is displayed in two different formats:
The following image displays the Types of Causes graph. The x-axis displays the types of cause (i.e., human, physical, and latent). The y-axis displays the number of RCA Hypothesis records that contain a cause in the State field, which is also viewed in the Logic Tree section.
The table below the graph displays information related to each RCA Hypothesis record that is linked to the RCA Analysis record.
The following table lists each item in the Cause Report and the corresponding RCA Hypothesis record field whose data is displayed in the report. A row exists for each RCA Hypothesis record and is categorized by the cause state (i.e., physical, latent, or human), which is stored in the State field of the RCA Hypothesis record.
Report Column | RCA Hypothesis Field |
---|---|
Hypothesis |
ID |
Hypothesis Description |
Description |
Confidence Factor |
Confidence Factor |
Copyright © 1993-2016 Meridium, Inc. All rights reserved.