When an RCA Hypothesis is created, the state is set to Hypothesis by default. Based on the Verifications, each RCA Hypothesis can then be tested and proven True or Not True, and then you can change the state of the Hypothesis accordingly.
Steps
In the design canvas, select the Hypothesis whose state you want to change, and then select
The Properties window appears, displaying the datasheet for the selected node.
Hint: You can also change the state of a Hypothesis from the States panel. To do so, select the Hypothesis, and then select
In the State list, select one of the following:
Select
The State of the Hypothesis is saved.
Copyright © 1993-2016 Meridium, Inc. All rights reserved.