This topic describes how to copy a Verification. You can also add a Verification node to the Logic Tree from the design canvas.
Steps
In the lower-left corner of the workspace, select the Verifications pane.
A list of Verifications that are available for the selected Hypothesis node appears.
Select the check box to the left of the Verification that you want to copy, and then select
Tip: You can copy more than one Verification.
The Copy Verification pane appears.
Select Save.
The Verification is saved to the database and linked to the Hypothesis and the selected RCA. The list of Verifications that appears on the Verifications tab is updated.
Copyright © 1993-2016 Meridium, Inc. All rights reserved.