When you create an RCA Failure Event, you are also defining the associated Failure Event node. After you create a Failure Event node, you cannot delete it via Root Cause Analysis, but you can modify the RCA Failure Event. Only one RCA Failure Event can be defined for each RCA.
Steps
In the left pane, select the Event Diagram tab.
A blank datasheet appears.
Select
The RCA Failure Event is created and linked automatically to the RCA. The Failure Event node appears in the design canvas.
Copyright © 1993-2016 Meridium, Inc. All rights reserved.