Critical Success Factors

The Critical Success Factors section of the Comprehensive Analysis report displays information that is stored in RCA Critical Success Factor records and important dates that are stored in the RCA Analysis record (e.g., the start date and publish date).

The following image shows an example of the Critical Success Factors section, outlined in red, as it appears in the Comprehensive Analysis report for the example RCA.

The Critical Success Factor section of the report

The following table lists each item in the Critical Success Factors section and the corresponding RCA Critical Success Factor or RCA Analysis record field whose data is displayed in the report.

Report Item Record Family Record Field

Critical Success Factors

RCA Critical Success Factor

CSF

Analysis Start Date

RCA Analysis

Start Date

Analysis End Date

RCA Analysis End Date

Date Published

RCA Analysis Date Published

Comments

RCA Analysis Comments

Copyright © 1993-2016 Meridium, Inc. All rights reserved.