Display the Logic Tree on Full Screen

The full screen view of the Logic Tree maximizes the Meridium Enterprise APM window, hides the frames around the design canvas, and displays only the Logic Tree and the Palette and Edit sections. The full screen view of the Logic Tree is useful for showing the Logic Tree in a presentation.

Steps

  1. Access the Logic Tree Diagram that you want to display in full screen.
  2. At the top of the workspace, in the Edit section, select .

    The Logic Tree appears in full screen. All of the options are available in the full screen mode.

    Note: You can return to normal mode from the full screen mode by selecting .

Copyright © 1993-2016 Meridium, Inc. All rights reserved.