Export a Logic Tree Diagram

You can export a Logic Tree as an image and save it to another location, such as your local hard drive.

Note: The zoom factor does not affect the size of the image that you want to export. Regardless of the zoom factor that is currently applied to the Logic Tree, the entire tree will be included in the image, even if part of the tree is cut off at the time you perform the export.

Steps

  1. Access the Logic Tree diagram that you want to export.

  2. At the top of the workspace, in the Edit section, select .

    The Save as window appears.

  3. Navigate to the location to which you want to save an image of the Logic Tree.

  4. In the File name box, enter the name of the file.
  5. In the Save as type list, select the format in which you want to save the image, and then select Save.

    Note: The above steps might change depending on the browser and browser settings that you use.

    The Logic Tree is saved to the selected location in the selected image format.

Copyright © 1993-2016 Meridium, Inc. All rights reserved.