The Verification Logs section of the Comprehensive Analysis report displays information that is stored in each RCA Verification record and the RCA Hypothesis record that is linked to an RCA Verification record. It also displays information stored in the Human Resource record that is linked to the RCA Team Member record that is linked to the RCA Verification record.
The following image shows an example of the Verification Logs section as it appears in the Comprehensive Analysis report for the example RCA.
The following table lists each item in the Verification Logs section and the corresponding RCA Verification, RCA Hypothesis, or Human Resource record field whose data is displayed in the report.
Report Column | Record Family | Record Field |
---|---|---|
Hypothesis |
RCA Hypothesis | ID |
Description |
RCA Hypothesis | Description |
Team Member |
Human Resource | First Name, Last Name |
Verification Method |
RCA Verification | Method |
Outcome |
RCA Verification | Outcome |
Copyright © 1993-2016 Meridium, Inc. All rights reserved.