The Verification Report displays information that is stored in each RCA Verification record and the RCA Hypothesis record that is linked to an RCA Verification record. It also displays information stored in the Human Resource record that is linked to the RCA Team Member record, which is linked to the RCA Verification record. The report includes each RCA Verification record that is linked to the RCA Analysis record.
The name of the analysis, which is stored in the Analysis Name field in the RCA Analysis record, is displayed at the top of the Verification Report. The following table lists each item in the report and the corresponding RCA Verification, RCA Hypothesis, or Human Resource record field whose data is displayed in the report.
Report Column | RCA Verification or RCA Hypothesis Record | Record Field |
---|---|---|
Hypothesis |
RCA Hypothesis |
ID |
Verification Method |
RCA Verification |
Method |
Outcome |
RCA Verification |
Outcome |
Responsible |
Human Resource |
First Name, Last Name |
Due Date |
RCA Verification |
Due Date |
Copyright © 1993-2016 Meridium, Inc. All rights reserved.