Access a Hazards Analysis

Steps

  1. Access the Hazards Analysis Overview page.

    Hint: You can also access the Hazards Analysis Overview page for a particular hierarchy level.

  2. In the workspace heading:

    The selected section appears, displaying a list of Hazards Analyses of the selected type.

    List of HAZOP Analyses

  3. Select the Hazards Analysis that you want to access.

    The Analysis Overview section appears, displaying the Risk Assessment graph.

    The Analysis Overview section of a HAZOP Analysis

  4. In the workspace, select the Definition tab.

    The datasheet for the Hazards Analysis appears.

    The HAZOP Analysis datasheet

  5. If needed, modify values in the available fields.

    Hint: You can modify a Hazards Analysis only if it is in the Planning state.

  6. In the upper-right corner of the datasheet, select .

    The changes made to the Hazards Analysis are saved.

Results

Copyright © 2017 General Electric Company. All rights reserved.