Hazards Analysis System/Node records store details on the group of equipment or functional locations that perform the process that you are studying. This topic provides an alphabetical list and description of the fields that exist for the Hazards Analysis System/Node family. These fields appear on the Hazards Analysis System/Node datasheet, unless otherwise specified. The information in the table reflects the baseline state and behavior of these fields.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site, and will then only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. See the Site Filtering section of the documentation for more information on using this feature.
| Field | Data Type | Description | Behavior and Usage |
|---|---|---|---|
|
Hazards Analysis Key |
Number |
A numeric value identifying the Hazards Analysis that is linked to the System/Node. |
This field does not appear on the datasheet. |
|
Modified By |
Character |
The name of the user who was logged in when the System/Node was last modified. |
This field does not appear on the datasheet. |
| Modified Date | Date | The date on which the System/Node was last modified. | This field does not appear on the datasheet. |
| Reference Drawing | Character | A value identifying the reference document. This value exists in the Name field in the corresponding Reference Document. | This field contains the IDs of the Reference Documents that are linked to the Hazards Analysis that is linked to the System/Node. |
| System/Node Comments | Text | Comments about the System/Node. | None |
| System/Node Description | Text | Description of the System/Node. | None |
| System/Node Equipment Type | Character | The type of equipment that corresponds to the system that the System/Node represents. | This field contains the System Codes in the MI Equipment Type System Code Table. |
| System/Node ID | Character | A brief description of the System/Node. | A value is required. |
| System/Node Number | Number | A numeric value representing the sequence in which the System/Node record appears. | This field is disabled and populated automatically. |
| System/Node Process Type | Character | The type of the process that you are studying. |
This field contains the following values:
|
Copyright © 2017 General Electric Company. All rights reserved.