The Risk Assessment feature is a combination of:
The Risk Assessment window, which is an interface that displays a Risk Matrix and other risk information.
-and-
The Risk Matrix data model, which includes entity families, relationship families, and records that determine:
The values that you will see in the Risk Assessment interface.
The baseline GE Digital APM database contains a set of baseline records that determine the values that you will see on the Risk Assessment window and the calculations that are performed using those values. You can access this window through modules such as:
If you do not want to use the baseline values and calculations, you can customize them or configure your own.
Hint: Refer to the Risk Matrix section of the end user documentation for additional information about understanding the Risk Matrix.
Copyright © 2017 General Electric Company. All rights reserved.