Consolidate Recommendations

If two or more recommendation records contain similar information, you can consolidate them into a single recommendation.

Note: After an RBI Recommendation record is consolidated, it cannot be modified.

Steps

  1. Access the Recommendation Management page.
  2. Next to the recommendations that will be involved in the Consolidate operation, select the check boxes.

  3. In the Recommendations pane, select , and then select Consolidate.

    The Consolidate Recommendations section appears.

    Note: Depending on the state configuration used for the Consolidate operation, a State Assignment window may appear. Select the appropriate Assignees from the State drop down menus listed, and then select Done. Recommendations that belong to the same asset can be consolidated.

  1. In the upper-right corner or the Consolidate Properties section, select Consolidate.

    The Actions Consolidated window appears, confirming that the Recommendations are consolidated.

  2. Select OK to close the window.

    Note: If you want to view the consolidate recommendations, select on the Recommendations pane, and then select Consolidated.

Results

Copyright © 2017 General Electric Company. All rights reserved.