The sections in this topic correspond to each step in the workflow for developing a Root Cause Analysis. In each section, the workflow for creating an RCA will be illustrated through examining the recurring failure(s) of a cooling water pump. The data used in each of the sections is listed in tables. In the tables, we list only the fields that contain a value. In the case of numeric fields, this includes fields that contain a value of zero (0). Fields that contain no value are not listed in the tables. The information in tables is provided for your reference.
Note: The information contained in these topics assumes that you are the user who will be performing the associated step in Root Cause Analysis and that all RCA administrative tasks have been completed.
Before you can begin conducting an RCA, you must establish the criteria that standardizes when an RCA should be performed. For example, the manager of the plant, where a cooling water pump exists, might specify criteria as:
If any pump fails one or more times per week for more than two successive weeks, regardless of the cost for repairs, an RCA study should be conducted.
-or-
Now, assume that in January 2015, the bearing temperature alarm, on the outboard bearing of a cooling water pump, sounded. By the time the operator arrived, the motor bearing temperature had increased to a point that the protective bearing temperature circuit caused the pump to shut down, resulting in loss of production. According to the criteria that was developed, these conditions dictate that an RCA should be performed. The first step is to create the analysis.
If water pump failure meets the criteria for requiring an RCA, the first step is to create the analysis. The user who will serve as the Principal Analyst can complete this step and initiate the development of the RCA for the recurring failures of the cooling water pump.
In the upper-right corner of the page, select New Analysis.
A blank datasheet appears in the Analysis Summary workspace.
Enter the values in the fields on the datasheet. For this example, you should create root cause analysis that contains the information as it appears in the following table:
Field | Value |
---|---|
Analysis Name | Cooling Water Pump |
Analysis Description | An analysis to determine the root cause of the pump overheating. |
Start Date | 01/06/2018 |
End Date | 01/15/2018 |
Comments | Comments |
Analysis Type | Mechanical |
Event Narrative | Investigate what caused the motor temperature in the water pump to increase and overheat. |
Cost | 20,000 |
Frequency |
1 Number 1 represents the number of failures that occurred for the cooling water pump |
Select
The Root Cause Analysis is saved.
In the workspace, select the Linked Assets tab.
The Linked Assets section appears.
Select
The Asset Finder window appears.
Search for PUMP and select it.
PUMP is listed in the Linked Assets section.
Select
The list of human resources appears in the left section and the list of team members appears in the right section.
The analyst, Suzie Jones, to help gather information surrounding the failure.
The mechanic, Pete Handy, because he will repair the cooling water pump.
The engineer, Bob Speck, because he is an expert on systems and safety guidelines.
Select
The selected names are added to the list of team members in the right section.
The Principal Analyst is Jane Doe, who is an expert on facilitating team discussion and documenting discussion notes.
Note: By default, the human resource that created an analysis will be added automatically as a team member and assigned the Principal Analyst role. You can change the Principal Analyst for an RCA.
In the workspace, select the Critical Success Factors tab.
The CSF section appears.
In the upper-left corner of the workspace, select
The Available CSFs and the CSFs for this Analysis subsections appear. The Available CSFs subsection contains the following Critical Success Factors that an administrative user has pre-configured for use with RCA:
In the workspace, select the Team Charter tab.
The Team Charter section appears.
In the box, enter the following text:
To identify the root causes of the cooling water pump failure. This includes identifying deficiencies in or lack of management systems. Necessary recommendations for root causes will be communicated to the management for rapid resolutions.
Select Done to save your changes.
The Team Charter section displays the Team Charter that you added.
You can preserve failure event data by creating an RCA Preserve Record, which contains a data-collection task that should be completed by the team member to whom the Preserve Record is assigned. Each task can be categorized according to the 5 P's (i.e., Parts, Paper, People, Position, Paradigms), which indicates the type of data that should be collected.
In the left pane, select the Preserve Records tab.
The Preserve Records workspace appears.
In the upper-left corner of the workspace, select
The New Preserve Record window appears.
In the Assigned to list, select the team member to whom you want to assign the Preserve Records, and then enter values in the available fields on the Preserve Records datasheet.
For this example, you should create RCA Preserve records that contain the information as it appears in each of the following tables:
RCA Preserve Record 1 | |
---|---|
Field | Value (s) |
Assigned To | Pete Handy |
Data Category | Parts |
Data to Collect | The pieces of the cooling water pump that could have caused the pump to overheat. |
Collection Strategy | Document (pictures and observations) the condition of the components of the pump. |
Date Due | 01/08/2018 |
Send Alert on Due Date? | True |
Days Before Due Date to Be Notified | 1 |
Frequency of Alert After Due Date | Daily |
Alert Email Body | This is a reminder to gather and document the pieces of the pump that could have caused the pump to overheat and report back to the team. |
Completed? | No |
Date Completed | N/A |
RCA Preserve 2 | |
---|---|
Field | Value (s) |
Assigned To | Suzie Jones |
Data Category | Paper |
Data to Collect | Standard operating procedures and frequent failure information |
Collection Strategy | Research |
Date Due | 01/9/2018 |
Send Alert on Due Date? | True |
Days Before Due Date to Be Notified | 1 |
Frequency of Alert After Due Date | Daily |
Alert Email Body | This is a reminder to gather the standard operating procedures and frequent failure information and report back to the team. |
Completed? | No |
Date Completed | N/A |
RCA Preserve Record 3 | |
---|---|
Field | Value (s) |
Assigned To | Bob Speck |
Data Category | People |
Data to Collect | Operating procedures used by those who maintain the pump. |
Collection Strategy | Interview the floor operators who are assigned to the pump. |
Date Due | 01/10/2018 |
Send Alert on Due Date? | True |
Days Before Due Date to Be Notified | 1 |
Frequency of Alert After Due Date | Daily |
Alert Email Body | This is a reminder to interview operators assigned to the pump and document their operating procedures and report back to the team. |
Completed? | No |
Date Completed | N/A |
RCA Preserve Record 4 | |
---|---|
Field | Value (s) |
Assign To | Bob Speck |
Data Category | People |
Data to Collect | Environment surrounding the pump. |
Collection Strategy | Tools, pictures, diagrams |
Date Due | 01/10/2018 |
Send Alert on Due Date? | True |
Days Before Due Date to Be Notified | 1 |
Frequency of Alert After Due Date | Daily |
Alert Email Body | This is a reminder to investigate the environment where the pump exists and report back to the team. |
Completed? | No |
Date Completed | N/A |
RCA Preserve Record 5 | |
---|---|
Field | Value (s) |
Assigned To | Jane Doe (Principal Analyst) |
Data Category | Paradigms |
Data to Collect | Common assumptions made when a pump fails. |
Collection Strategy | Research and interview. |
Date Due | 01/10/2018 |
Send Alert on Due Date? | False |
Completed? | No |
Date Completed | N/A |
After each team member has collected the data that is specified in the RCA Preserve Record, they should record their findings for the rest of the team through artifacts, including Reference Documents and hard copies of documents. After all the RCA Preserve Records have been completed, the team can begin to analyze the data.
After the team has preserved the failure data, the team can begin to analyze the data. To help you visualize the event and organize the team's hypotheses and analysis, you should create an Event Diagram or a Logic Tree depending on your requirement. For our example, we will create a Logic Tree diagram.
In the left pane, select the Logic Tree tab.
A blank datasheet appears.
Enter the following values:
Field | Value (s) |
---|---|
Event End Date | 01/15/2018 |
Event ID |
RCA-01/15/2018 Note: The Event ID field is populated automatically with the date the is created and is disabled so that value cannot be changed. If you choose to re-create this example RCA Event, your Event ID value will be different from the value listed here. |
Event Start Date | 01/06/2018 |
Label | Overheating in Pump 1 |
Long Description | Investigate the cause of a cooling water pump to overheat and shut down the system. |
Select
The Failure Event node appears in the design canvas in the Logic Tree workspace.
Select the Failure Mode that you added.
The Properties window appears.
Enter the following information to define the Failure Mode, and then select
RCA Failure Mode ID | Value (s) |
---|---|
No Spare Parts |
Label: No Spare Parts Description: No spare parts caused the pump to be out of commission for a longer amount of time. |
Add another Failure Mode using the following information:
RCA Failure Mode ID | Value (s) |
---|---|
Motor tripped due to high temperature. |
Label: Motor tripped due to high temperature. Description: The motor shut off because the temperature became too hot and the system was shut down. |
Diagram the events that led up to and immediately followed the failure event. For this example, you would create the Event Diagram as shown in the following image. The team should note the trend in the failures that occurred in the past. In this way, the team may be able to identify a pattern in the events prior to the RCA that may indicate the underlying cause(s) for these failures.
This example contains nine RCA Sequence Nodes, which are displayed on the Event Diagram.
For each RCA Sequence Node, the following table lists the type of node and the values that exist in the RCA Sequence Node.
Type of Node | Values |
---|---|
Start/Finish |
Label: Pump place into service Event Start Date: 1/1/2014 12:00 AM Event End Date: 1/1/2014 12:00 AM |
Process |
Label: Cooling water pump turned on daily Event Start Date: 1/1/2014 12:00 AM Event End Date: 1/6/2015 12:00 AM |
Operation |
Label: Bearing Temperature Alarm sounded Event Start Date: 1/6/2015 12:00 AM Event End Date: 1/6/2015 12:00 AM |
Operation |
Label: Pump Overheated Event Start Date: 1/6/2015 12:00 AM Event End Date: 1/6/2015 12:00 AM |
Operation |
Label: System shut down Event Start Date: 1/6/2015 12:00 AM Event End Date: 1/6/2015 12:00 AM |
Decision |
Label: Decided to perform an analysis Event Start Date: 1/6/2015 12:00 AM Event End Date: 1/6/2015 12:00 AM |
Start/Finish |
Label: RCA Study began Event Start Date: 1/6/2015 12:00 AM Event End Date: 1/16/2015 12:00 AM |
Select the Hypothesis that you added.
The Properties window appears.
Enter the following information to define each of the Hypotheses required for our example.
RCA Hypothesis ID | Value (s) |
---|---|
Level 1 | |
Mechanical |
Label: Mechanical Descriptions: The increase in temperature was due to a mechanical failure. Confidence Factor: Likely (3) State: Hypothesis True |
Electrical |
Label: Electrical Descriptions: The increase in temperature was due to an electrical failure. Confidence Factor: Possibly True (2) State: Hypothesis Not True |
Level 2 | |
Outboard bearing |
Label: Outboard bearing Descriptions: The outboard bearing had a mechanical problem. Confidence Factor: Highly Likely (4) State: Hypothesis True |
Inboard bearing |
Label: Inboard bearing Descriptions: The inboard bearing had a mechanical problem. Confidence Factor: Somewhat True (1) State: Hypothesis Not True |
Level 3 | |
Erosion |
Label: Erosion Descriptions: The outboard bearing eroded after overuse. Confidence Factor: Somewhat True (1) State: Hypothesis Not True |
Corrosion |
Label: Corrosion Descriptions: The outboard bearing corroded and was rusty. Confidence Factor: Somewhat True (1) State: Hypothesis Not True |
Fatigue |
Label: Fatigue Descriptions: The outboard bearing was overheated due to a weakness of materials. Confidence Factor: Highly Likely (4) State: Hypothesis Not True |
Level 4 | |
Misalignment |
Label: Misalignment Descriptions: The outboard bearing was not aligned correctly. Confidence Factor: Possibly True (2) State: Hypothesis Not True |
Loose Bolts |
Label: Loose Bolts Descriptions: Bolts were loose and caused the outboard bearing to become loose. Confidence Factor: Possibly True (2) State: Hypothesis Not True |
Lubrication Issue |
Label: Lubrication Issue Descriptions: The outboard bearing was not receiving the right amount of lubrication. Confidence Factor: Highly Likely (4) State: Cause Physical |
Level 5 | |
Leak |
Label: Leak Descriptions: The lubricant was leaking from the pump. Confidence Factor: Possibly True (2) State: Hypothesis Not True |
Too Much Applied |
Label: Too much applied Descriptions: There was too much lubricant, causing, the bearing to operate too quickly and overheat. Confidence Factor: Possibly True (2) State: Hypothesis Not True |
Too Little Applied |
Label: Too little applied Descriptions: There was not enough lubricant, causing friction and an increase in temperature. Confidence Factor: Likely (3) State: Cause Human |
Level 6 | |
Poor Training |
Label: Poor training Descriptions: Workers were not properly training on applying lubricant to the bearing. Confidence Factor: Possibly True (2) State: Hypothesis Not True |
Inadequate Procedures Documented |
Label: Inadequate Procedures Documented Descriptions: Workers are referencing procedure documentation that is not clear. Confidence Factor: Possibly True (2) State: Hypothesis Not True |
Worker Fatigue |
Label: Worker Fatigue Descriptions: Workers are overworked and are not able to perform at an acceptable level. Confidence Factor: Likely (3) State: Cause Physical |
Inadequate Accountability of Workers |
Label: Inadequate Accountability of Workers Descriptions: Workers are not being held accountable for the maintenance procedures they are required to perform. Confidence Factor: Highly Likely (4) State: Cause Latent |
Diagram each failure mode in detail. For this example, you would create a Logic Tree like the one shown in the following image:
In the Logic Tree in this image, you can see that two Failure Mode nodes are linked to the Failure Event node, and multiple Hypothesis nodes are linked to the Motor Tripped due to high temperature Failure Mode node.
This example contains four RCA Logic Gates, which represent Logic Gate nodes and are used in the Logic Tree. You must enable Logic Gates to view them on the Logic Tree.
In the following table, the Logic Gates are numbered as they appear in the Logic Tree from left to right. For each RCA Logic Gate, the table displays the value in the Gate Type field of the RCA Logic Gate and identifying information about the node (e.g., RCA Failure Mode) to which it is linked.
RCA Logic Gate | Value Specified | Linked To |
---|---|---|
1 |
Gate Type: OR |
RCA Failure Mode: Motor tripped due to high temperature RCA Hypothesis: Mechanical RCA Hypothesis: Electrical |
2 |
Gate Type:OR |
RCA Failure Mode: Motor tripped due to high temperature RCA Hypothesis: Mechanical RCA Hypothesis: Inboard bearing RCA Hypothesis: Outboard bearing |
3 |
Gate Type:OR |
RCA Failure Mode: Motor tripped due to high temperature RCA Hypothesis: Outboard bearing RCA Hypothesis: Corrosion RCA Hypothesis: Erosion RCA Hypothesis: Fatigue |
4 |
Gate Type:OR |
RCA Failure Mode: Motor tripped due to high temperature RCA Hypothesis: Fatigue RCA Hypothesis: Loose Bolts RCA Hypothesis: Lubrication Issue RCA Hypothesis: Misalignment |
5 |
Gate Type:OR |
RCA Failure Mode: Motor tripped due to high temperature RCA Hypothesis: Lubrication Issue RCA Hypothesis: Leak RCA Hypothesis: Too Little Applied RCA Hypothesis: Too Much Applied |
6 |
Gate Type:OR |
RCA Failure Mode: Motor tripped due to high temperature RCA Hypothesis: Too Little Applied RCA Hypothesis: Inadequate Accountability of Workers RCA Hypothesis: Inadequate Procedures Documented RCA Hypothesis: Poor Training RCA Hypothesis: Worker Fatigue |
Now that several likely hypotheses have been introduced, the team will need to rule out hypotheses. To rule out a hypothesis or prove a hypothesis, the hypothesis will need to be tested against the data that is available to the team (i.e., the failure event data and the team of experts).
As described in the next step, the Principal Analyst should create RCA Verifications and assign them to team members who will be responsible for completing the associated task.
In the lower-left corner of the workspace, select the Verifications tab.
The Verifications pane appears.
Above the list, select
The Create Verification pane appears.
In the Assigned to list, select the team member to whom you want to assign the Verification.
A blank datasheet appears.
Enter the details in the available fields based on the following information to define each of the Verification required for our example, and then select
RCA Verification ID | Values Specified |
---|---|
Inspect wiring to make sure that the cause was not electrical. |
Due Date: 1/10/2015 Method: Inspect wiring to make sure that the cause was not electrical. Completed: No |
Perform a metallurgical analysis to determine why the bearing failed. |
Due Date: 1/10/2015 Method: Perform a metallurgical analysis to determine why the bearing failed. Completed: False |
The following image shows an example of an RCA Verification that contains a task to test the Mechanical hypothesis.
The task defined in this RCA Verification instructs the team member to inspect the wiring for the cooling water pump to ensure that the problem was not electrical, but mechanical.
When a hypothesis has been tested, you must change the state of the associated RCA Hypothesis, as described in the next step.
For example, the following image shows the Logic Tree after Pete Handy has completed the RCA Verification to which he was assigned. Pete Handy concluded that the wiring did not the cause the pump to overheat, so the problem must be mechanical.
After the state of the Mechanical RCA Hypothesis is set to True, the team can continue down the Logic Tree until they identify the root cause. Causes can be further identified as physical, human, or latent. For example, the following image shows the Logic Tree after ALL the RCA Verifications have been completed. The team has concluded that inadequate accountability of workers has led to insufficient lubricant being applied to the outboard bearing, which caused the motor's temperature to increase and the pump to overheat.
In this case, the root cause for the pump failure would be identified as latent (i.e., inadequate accountability of workers), which lead to human (i.e., too little applied) and physical (i.e., lubrication issue) causes. Now that a hypothesis has been verified and the root cause has been determined, you can create RCA Recommendations to communicate your findings on how to prevent this failure in the future.
If the hypothesis is not true but you cannot rule out the hypothesis and set the state to False, you can assign a probability to the hypothesis to include the team in determining the possibility of the hypothetical cause.
Now that the team has determined the root cause of the cooling water pump failure to be inadequate accountability of workers, you will want to record your findings and create RCA Recommendations. After recommendations have been implemented, you can share the results of the RCA with others. You can access the RCA Overview page to view the financial effects of implementing the recommendations. For our example, we will create one Recommendation record.
In the upper-right corner the workspace, select the
The Recommendations pane appears.
Select
The RCA Recommendation datasheet appears.
On the General Information tab, enter the following details in the available fields:
Field | Description |
---|---|
Alert Responsible Party When Due? |
True |
Analysis ID |
Cooling Water Pump |
Assigned to Name |
Suzie Jones |
Author Name |
Jane Doe |
Business Impact |
Production (PRODUCTION) |
Cause |
Inadequate accountability of workers. |
Cause Type |
Cause Latent |
Days Before Due Date To Be Alerted? |
4 |
Final Approver Name |
Jane Doe |
Frequency of Alert After Due Date |
Daily |
Implementation Alert Text |
You have less than 4 days to complete the new required report. |
Mandatory Date |
2/28/2015 |
Recommendation Description |
This report will require workers to document each time they perform a routine procedure, which will hold them accountable for pump maintenance. |
Recommendation Headline |
Create a new performed maintenance report. |
Recommendation ID |
REC-1376 |
Recommendation Priority |
Medium (Medium) |
Required Equipment Status |
On-Line (ON-LINE) |
Reviewer Name |
Jane Doe |
Status |
Created (CREATED) |
Target Completion Date |
Monday, February 20, 2015 |
If you want to schedule a recommendation alert email to be sent to a specified recipient, select the Alert tab, and enter the necessary information on the datasheet.
Select
The RCA Recommendation is saved to the database and linked to the analysis for the selected Root Cause analysis.
After you have successfully identified the root causes associated with the failure that was investigated, you can communicate the findings and propose recommendations to the appropriate individuals within your organization. You can communicate the findings via a hyperlink to the analysis or via a summary report through email to selected recipients.
After the RCA findings have been communicated and the recommendation has been implemented, the team will want to track the effectiveness of the recommendation to see if the new report has prevented the cooling water pump from failing thus far. Tracking for results involves creating RCA Tracking Items, scheduling the Tracking Evaluations in the GE Digital APM Schedule Manager, and modifying the existing recommendation or creating a new one based on the discoveries that are made through reevaluation.
For our example, we will create one tracking item.
In the left pane, select the Track tab.
The Track workspace appears.
In the upper-left corner of the workspace, select
The Add/Edit Tracking Item window appears, displaying a blank datasheet.
Enter the following information in the available fields:
Field | Description |
---|---|
Active |
True |
Start Date |
3/1/2015 |
Count |
2 |
Cost |
10,000 |
Alert |
Williams, Bob Note: Williams, Bob will receive an e-mail that alerts him that the performance of the cooling pump has again fallen below the tolerable limits or that the corrective actions from the first RCA were ineffective. |
Message Subject |
Cooling Water Pump Improvement |
Message Text |
Cooling water pump 1 has failed and needs to be re-evaluated. The reason for the failure is that the performance of the cooling pump has again fallen below the tolerable limits or that the corrective actions from the first RCA were ineffective. |
Select
The Tracking Item is saved.
Copyright © 2017 General Electric Company. All rights reserved.