Probability Distribution
About Site Filtering in Probability Distribution Analysis
In Probability Distribution, the site is assigned based on the user's selection in the Site control, but the data for the analysis can be generated by a query that contains records from multiple sites.
Analyses that are created for a single site and that are based on a query containing multi-site data will contain multi-site data. A single-site user with access to the analysis can open the analysis and view all of the multi-site data in an analysis.
Consider an organization that has three sites, Site X, Site Y, and Site Z. The following Probability Distribution records exist:
- Probability Distribution A: Assigned to Site X
- Probability Distribution B: Assigned to Site Y
- Probability Distribution C: Assigned to Site Z
- Probability Distribution D: No site assigned (global record)
Scenario 1: User assigned to only Site X
This user will see Probability Distributions A and D.
Scenario 2: User assigned to both Site X and Site Y
This user will see Probability Distributions A, B, and D.
Scenario 3: Super User
This user will see Probability Distributions A, B, C, and D.
Probability Distribution Analysis Data Model
The following diagram shows how the families used in Probability Distribution Analysis are related to one another.

In the above image, the Distribution box represents one of four Distribution subfamilies in which records can exist: Normal, Weibull, Exponential, Lognormal, Triangular, Gumbel, or Generalized Extreme Value.
As you develop a Probability Distribution Analysis, you will create records in these families and link them together, either manually or automatically via the options in the GE Digital APM Framework. Throughout this documentation, we use the term Probability Distribution Analysis to mean the combination of the Distribution record and all the records that are linked to it.
About Data Mapped to the Baseline Analysis <Source Type> Window
When you create a Probability Distribution Analysis from a query or dataset, the Probability Distribution Builder window will prompt you to map values from columns in the query or dataset to certain values in the Probability Distribution Analysis. The values that you select to map on the Select Data Fields screen in the Probability Distribution Builder window will then appear in the associated columns in the Baseline Analysis <Source Type> window. The <Source Type> is Query or Dataset on which your analysis is based.
This family is enabled for site filtering, which means that records in this family can be assigned to a specific site and will only be accessible to users who are assigned to the same site and have the appropriate license and family privileges. For more information, refer to the Sites section of the documentation.
Details
The following table displays which columns are mapped from fields in the Probability Distribution Builder window to columns in the Baseline Analysis <Source Type> window:
| Probability Distribution Builder Screen | Probability Distribution Builder Field | Baseline Analysis <Source Type> Window Column |
|---|---|---|
| Select Data Fields | Value | X |
| Select Data Fields | Censored | Censored |