Trend Chart Overview
The trend chart widget allows you to plot real time data and historical data from Historian servers. You can plot the data using the context of a model or browse for a Historian server. You can then add tags to the chart.
The model contains asset types and assets. The assets have properties associated with them, which are, in turn, associated with tags defined in Historian.
The following image shows an example of a trend chart.
Task | Procedure |
---|---|
Access the properties used in a trend chart. | The properties used in a trend chart appear in the Legend section. |
Remove a property from a trend chart. | In the Legend section, in the row containing the property, select ![]() |
Increase the area of a trend chart. |
|
Pause the data flow of a trend chart. | In the toolbar, select ![]() ![]() |
View the delta value between two data points. | In the toolbar, select ![]() |
Drill down a trend chart. | In the toolbar, select ![]() ![]() If you want to zoom in or zoom out a single axis, select the axis in the drop-down list box adjacent to If you want to enlarge an area on the chart, select |
Pan across a trend chart. | In the toolbar, select ![]() |
Mark a trend chart view as favorite. It is an easy way to view the trend chart for commonly used configuration settings. | In the toolbar, select ![]() ![]() |
View the statistics of tags plotted on a trend chart. | In the toolbar, select ![]() ![]() |
Export the trend chart data. | In the toolbar, select ![]() ![]() |
Print a trend chart. | In the toolbar, select ![]() ![]() |
Reset the trend chart options. | In the toolbar, select ![]() ![]() |
Recommendations While Using a Trend Chart
- When you add a trend chart to a page using the page designer, use separate containers for the breadcrumb and the chart. For the trend chart, set the height to 100%.
- When accessing a trend chart on a mobile device:
- Use a device with medium to high resolution.
- Use the device in landscape mode.
- To print a trend chart using an Android device, use the screen capture feature rather than selecting
.
- Configure the trend chart using a desktop rather than an Android device. This is because when you attempt to search for an asset or a Historian tag on an Android device, the in-built keyboard of the device appears, which may not allow you to enter the search criteria.
- When you view the delta between two data points, the value may not be clearly readable on a mobile device with low to medium resolution. Therefore, we recommend that you view the delta value on a desktop or a mobile device with high resolution.
- When you view statistical data, the trend chart area may be limited. To avoid this issue, plot up to two properties on the trend chart.
- To pan across the trend chart or drill down the trend chart on an iPad, use the Zoom feature of the iPad rather than selecting
,
, or
, respectively.