You do not have the latest version of Operations Hub! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Operations Hub product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Create an Action to Send a Command to a Device
About this task
This topic describes how to create an action to send a command to a device. You can also create an action to:
Enter or select values as described in the following table.
Option
Description
Function
Select Send_MQTT_Command to send a command to a device that is configured with IQP MQTT. The Input Source and Value boxes appear for topic and payload.
Input Source
Select Fixed value if you want to send a fixed value to the device when the event is triggered.
Value
Enter the fixed value that you want to send to the device when the event is triggered.
Allow End User to set value
Select this check box if you want application users to set the value, and then enter a name in the Input Name box that appears.
Scheduler
Select one of the following options:
Take action only on initial trigger: Select this option if you want to send the command after switching from the state of not meeting the condition to meeting the condition. By default, this option is selected. For example, suppose you have created an action to send the command when the temperature recorded by a device exceeds 40 degrees Celsius. Suppose the temperature recorded by the device is as follows: 35, 38, 41, 45, 39, 42. In this scenario, the command is sent when the temperature is 41 and 42.
Take action on every trigger: Select this option if you want to send the command every time the event is triggered. For example, suppose you have created an action to send a command when the temperature recorded by a device exceeds 40 degrees Celsius. Suppose the temperature recorded by the device is as follows: 35, 38, 41, 45, 39, 42. In this scenario, the command is sent when the temperature is 41, 45, and 42.
Select Save or Save and Exit.
The event template is created.
Results
When the event is triggered, the command is sent to the MQTT broker.