You do not have the latest version of Operations Hub! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Operations Hub product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Create an Email Template
About this task
This topic describes how to create an email template. You can also copy an email template.
Procedure
In the main navigation menu, selectEMAILS.
The EMAILS workspace appears.
Select Add new email template.
The Create Email Template window appears.
Enter a value in the Email Template Name box, and then select Create. The name must contain at least one uppercase or lowercase letter.
The Subject, Body, and URL sections of the email template appear.
In the Subject, Body, and URL sections, select the options for which you want to add details.
Option
Description
Add Text
When you select Add Text, a text box appears in the corresponding section. You can enter the text that you want to include in the email template.
Add Parameter
Parameters allow you to add dynamic content to the email based on values from the event. When you select Add Parameter, a drop-down list box appears in the corresponding section. You can select the parameter that you want to include in the email template.
Add Paragraph
When you select Add Paragraph, a resizeable text box appears in the corresponding section. You can enter the text that you want to include in the email template. You can add a paragraph only in the Body section.
Add Newline
When you select Add Newline, a line appears after the current element.
As needed, in the URL section, enter a URL that you want to include in the email template.