You do not have the latest version of Operations Hub! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Operations Hub product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Create a Relationship Between Entities
About this task
You cannot use a baseline entity or a pivot entity as a source entity. You can, however, use it as a target entity.
Procedure
In the main navigation menu, selectENTITIES.
The ENTITIES workspace appears.
Optional: Select the check boxes of the entities for which you want to create a relationship.
Select DESIGNER.
The DESIGNER section appears, displaying all the entities created in the site. If, however, you have selected entities in the previous step, only the selected entities appear. If a relationship exists between two entities, a line connecting them appears.
Tip: You can arrange the entities in an order, minimize all entities, maximize all entities, or maximize only the entities in a relationship by selecting Auto Arrange, Minimize All, Maximize All, or Maximize linked Entities respectively.
Next to each entity for which you want to create a relationship, select .
A list of fields in each entity appears.
Select Add Relationship, and then select a field from the source entity and then the target entity.
A relationship is created between the entities. A line connecting both the entities appears.