You do not have the latest version of Operations Hub! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Operations Hub product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Uninstall Operations Hub on Windows
Procedure
If you want to uninstall Operations Hub automatically, open Command Prompt, and enter the following command: <Installation folder path of Operations Hub>\OpHub-Windows_Installer>ophub_bundle -uninstall
If you want to uninstall Operations Hub manually, perform the following steps:
On the machine on which you want to uninstall Operations Hub, select Control Panel > Uninstall a Program.
A list of programs that you can uninstall appears.
Right-click Operations Hub, and then select Uninstall.
The Uninstall Options page appears.
In addition to uninstalling Operations Hub, if you want to delete all the related data and applications, select the Purge databases during uninstall check box.
Select Next.
The You are ready to uninstall page appears.
Select Uninstall.
Results
Operations Hub is uninstalled from the Windows machine.