Click here to check out all the new features in the latest version of Operations Hub. Let Operations Hub help you centralize and digitize your industrial applications.
Important: You do not have the latest version of Operations Hub! You are missing out on the newest capabilities and enhanced security. For information on all the latest features, see the Operations Hub product page. For more information on upgrades, contact your Proficy sales agent or e-mail Proficy Sales Support. For the most up-to-date documentation, go here.
Modify Settings
Procedure
In the main navigation menu, selectAPPS.
The APPS workspace appears.
In the Name column, select the application whose settings you want to modify.
The PAGES workspace appears.
In the main navigation menu, selectSETTINGS.
The SETTINGS workspace appears.
As needed, modify values as described in the following table.
Field
Description
Show extended error information
Select this check box if you want detailed error information to appear in error messages. You can use this information to troubleshoot issues in the application.
Show trace button
Select this check box if you want to display a button that allows you to access information on the data retrieved from queries, functions, and global variables that are used in the application. It also includes data that is inserted or updated using queries. When you select this check box (and save your changes), a Trace appears in the application. You can select this button to view the trace information.
Hide loading in application
Select this check box if you do not want to display a busy indicator to indicate that a page is loading data from a query.
Hide application title
Select this check box if you do not want the title of the application to appear when you access the application.
Show User Pages
Select this check box if you want to display user pages in the application navigation menu. These pages are used to change the password of the user and access user settings using the application. If you select this check box, the option to access the user pages appears in the application title. If, however, the Hide application title check box is selected, the option is moved to the navigation menu of the application.
Auto-dismiss Errors
Select this check box to automatically
dismiss error messages after 3-5 seconds if they
pop up in the end application. Recommended for
hands-free environments.