Reliability Distribution: Workflow
Reliability Analytics: Reliability and Probability Distribution Analysis Workflow
This workflow describes the process for analyzing changes to a measured value over time to determine the mathematical median and mean values associated with analyzed data.
In the following workflow diagram, the blue text in a shape indicates that a corresponding description has been provided in the sections that follow the diagram.

Existing Analysis?
Persona: Analyst
Is the analysis one that was created previously and saved to the database?
View Existing Analysis
Persona: Analyst
View the details of an existing analysis.
Create Analysis
Persona: Analyst
Create an analysis based on production data or event data.
Review/Modify Distribution Parameters
Persona: Analyst
If Distribution Parameters have been updated, review/modify them. Distribution Parameters are updated when a different distribution type is selected (e.g., when changing from Lognormal to Auto).
Optimize Preventative Maintenance
Persona: Analyst
Determine the optimal time to perform Preventive Maintenance based on a failure rate.
View Report
Persona: Analyst
View and save the analysis report.
Manage Performance Recommendations
Persona: Analyst
Create any number of performance recommendations and Approve them using state management.
Go to the Manage Performance Recommendations workflow.
Other Workflows
Persona: Analyst
Other workflows provide production data from SAP, EAM, and Recommendations.