Viewing Batch Genealogy

To_view_the_Batch_Genealogy | Using_the_report

This application shows the genealogy for a selected batch. From this report, you can see the individual phases that make up an operation, the individual operation(s) that make up the unit procedure and the unit procedure that makes up the batch.

To view the Batch Genealogy

  1. Search for your saved Batch Analysis.

  2. In the Query Results page, click the radio button next to the desired batch.

  3. Under Single Batch, click the View Batch Genealogy hyperlink.

Using the report

The gray boxes indicate that there are additional procedural elements that are not being displayed. In the example above, the gray box with the number 8 in it indicates that there are eight phases that make up the operation. To view the phases, double-click the green box that is pointing to the gray box.

The green boxes represent the procedural elements that make up the batch.

  • U = Unit Procedure

  • O = Operation

  • P = Phase

The three small alarm boxes inside the green procedural element box indicate the number and level of alarms. To view the Alarm List by Units web part, select the procedural element ( green box), and click the desired alarm box.

  • The left box indicates the number of High alarms.

  • The middle box indicates the number of Medium alarms.

  • The right box indicates the number of Low alarms.

To go to a different batch, type the batch name in the box and click the Go button.

To view detail for a specific procedural element, select the appropriate green box and then click the View Detail button.

To select a different input or output unit, click the Filter on Unit button.

See Also