Creating a Batch Analysis

You can create a new Batch Analysis from either the Plant Applications Web Administrator or the Plant Applications Web Report Server.

Before you can use the Batch Analysis Web report, you will need to configure your Plant Applications Plant Model and configure the Plant Applications GBDB database to read your batch records. For more information, please see, Introduction to Batch Analysis.

Batch units are enclosed with angle brackets, < >.

To create a new Batch Analysis from the Plant Applications Web Administrator

  1. Log in to the Plant Applications Administrator.

  2. Open Server Management.

  3. Double-click on Administer Web Server.

  4. In the Web Server Administrator, open the Web Content folder.

  5. Right-click on Batch Analysis and select View from the pop-up menu.

  6. In the Saved Batch Analysis page, click the Create New icon to create a new batch analysis.

  7. Make your changes in the Analysis Properties dialog box.

To create a new Batch Analysis from the Plant Applications Web Report Server

  1. Log on to the Plant Applications Web Report Server.

  2. Expand the Report Tree.

  3. Click on Batch Analysis. (If Batch Analysis is not in your Report Tree, please see your Plant Applications Administrator).

  4. In the Saved Batch Analysis page, click the Create New icon to create a new batch analysis.

  5. Make your changes in the Analysis Properties dialog box.

See Also