Variable Scatter Analysis
This ASP application creates a scatter plot to help you evaluate variables by providing a visual picture of the relationship between two variables. The pattern of the points helps indicate the type and strength of the relationship between the two variables. The following parameters are required:
-
The start and end time
-
The variables
After you run the report, you can select a product from the drop-down list. Click the Properties icon to change the time period, select different variables and specify which variable is the primary variable (the variable that determines the timestamp for gathering the other variable data). You can also display a trend line and connect all points on the chart.