Line Time Accounting

This application displays the timeline of selected events over multiple production units during a specified period of time. You can select production units from multiple production lines. This report requires the following parameters:

  • The start and end time

  • The production units

  • The event types

Click the Properties icon to open the dialog box where you can change the time period, the units, and the events included in the report.

Line Time Accounting Report

You can click each event to view the Event Detail report. You can hover over an event to view additional information about the event.

See Also: