Mobile Application
About the GE Digital APM Mobile Application
GE Digital APM provides a mobile app that can be installed on iOS, Android, and Windows devices.
This app offers certain APM functionality designed specifically for use offline and includes the following modules:
- Inspection Management and Inspection Field Data Collection
- Mobile Proof Testing
- Rounds Data Collection
- SIS Management
Note: The Rounds Pro module provides the Rounds Pro mobile application which can be installed on hand-held devices and allows you to collect data. For more information, refer to the Rounds Pro Mobile App section of the Rounds Pro documentation.
Mobile Application Supported Operating Systems
Supported Operating Systems
Important:
- Any management policy applied to mobile devices must be set up to allow the required permissions for the GE Digital APM mobile application. If restrictions are placed on iOS, Windows, or Android devices by a global policy or mobile device management system, device storage, scanning, photography, location services, and other functionality may be disabled.
- If you are using a Windows device, ensure that Windows App Store access is enabled.
- Ensure that the application is distributed to all relevant devices.
The following table lists the operating systems and corresponding versions that the GE Digital APM mobile application supports.
Operating System | Version(s) Supported |
---|---|
iOS | 12, 13, and 14 |
Android | 7, 8, 9, 10, and 11 |
Windows | Windows 10 (64 bit) |
Note: The method used to access Reference Documents in the GE Digital APM mobile application will vary depending on your device platform. For example, on Windows and Android devices, the first time you access Reference Documents, you will be prompted to select the application in which you want to open a file, and this selection will then become the default. Apple iOS will always prompt you to select an application. On all platforms, you will also be prompted when the platform for your device does not recognize the file type that it is attempting to download.
Install the GE Digital APM Mobile Application on an iOS Device
GE Digital provides an iOS application, but there are specific steps that you must perform to install the GE Digital APM mobile application on iOS devices.
Before You Begin
An Apple developer's license must be purchased.
Procedure
Install the GE Digital APM Mobile Application on an Android Device
GE Digital provides an Android application, but there are specific steps that you must perform to install the GE Digital APM mobile application on Android devices.
Procedure
Install the GE Digital APM Mobile Application on a Windows Device
Procedure
Access GE Digital APM via the Mobile Application
Procedure
Access the GE Digital APM Mobile Application Using Single Sign-On (SSO)
This topic describes how to access the GE Digital APM mobile application using SSO.