Exceptions
About Exceptions
Exceptions are action items that must be completed by the team before delivering a change. In the Application Settings for MOC, you can create Exception records to identify the type of Exception that must be created for an Answer Option. When you respond to Questions in a Checklist in the Change Project, Exceptions are automatically created by copying the Exceptions that you created.
Default Exceptions in MoC
GE Digital APM provides a set of Exceptions, by default. These Exceptions are associated with Answer Options of Questions. The following table lists the default Exceptions, which you can modify as needed:
| Exception ID | Exception Type |
|---|---|
| Asset Change | Update EAM/CMMS records |
| Asset Removal | Update EAM/CMMS records |
| Chemical Change | Update facility chemical hazard storage documentation |
| Controls parameters | List all pre and post change controls parameters |
| Electrical load | Update electrical safe work plans |
| Energy Source | Update LOTO documentation and safe work plans |
| Exit Route | Revise or replace emergency exit route placards |
| Flare addition | Update flare usage documentation |
| Heights | Update safe work plans related to working above grade |
| Lock out Tag out | Update safe work plans, and applicable LOTO plans |
| Machine guarding | Revise existing or add new machine guarding as app |
| Material Storage | Update facility chemical hazard storage documentation |
| MSDS | Update material safety data sheet |
| Procedural | Update applicable Operating or Maintenance procedure |
| Process Sewer | Update sewer source and usage documentation |
| Solid Waste | Update facility chemical hazard storage documentation |
| Storm Drain | Notify local authorities, and update facility possible discharge documentation |
| Update and link all updated drawings and diagrams | Drawings/Diagrams |
| Update applicable emergency evacuation routing | Ingress/Egress |
| Update the process safety information | Process Safety Information |
to save your changes. The changes made to Exceptions in the administrative settings for MOC will not affect the Change Projects that have used the Exceptions prior to modification.
.
button is enabled.