Query Sources, Fields, Joins, and Hyperlinks
About Query Sources, Fields, Joins, and Hyperlinks
The following topics describe available actions related to query sources, fields, joins, and hyperlinks.
Add a Source
About This Task
Steps: Add a Source to a New Query
Procedure
- To add a source to a new query:
- To add a related source:
What To Do Next
Add a Field to a Query
Procedure
Results
- The Field cell contains a drop-down list, where you can modify your field selection.
What To Do Next
Arrange Columns
Procedure
Modify the Properties of a Join
Procedure
- To modify a join:
Option Description Inner join Represented by the Only include rows that are linked through '<Relationship Family>' option. Left outer join Represented by the Include ALL rows from '[<predecessor source>]' and only those rows from '[<successor source>]' where the joined fields are equal option. Right outer join Represented by the Include ALL rows from '<Successor Family>' and only those rows from '<Predecessor Family>' that are linked through '<Relationship Family>' option. Option Description Inner join Represented by the Only include rows that are linked through '<Relationship Family>' option. Left outer join Represented by the Include ALL rows from '[<predecessor source>]' and only those rows from '[<successor source>]' where the joined fields are equal option. Right outer join Represented by the Include ALL rows from '<Successor Family>' and only those rows from '<Predecessor Family>' that are linked through '<Relationship Family>' option. - To modify a manual join:
Delete a Join
Procedure
Display the System and Inactive Fields for a Query Source
Procedure
Remove a Query Source
Procedure
Create a Hyperlink
Procedure
- To create an internal URL:
- To create an external URL:
Results
Note: If you clear the Included check box for the System field, and then run the query in formatted mode, selecting a hyperlink in the query results may cause the following error message to appear: An entity with the key '{<X>}' could not be found. Please close the tab. If this occurs, select the Included check box for the System field, and then rerun the query.
- You cannot modify a hyperlink using the URL Builder window. The URL Builder interface does not store settings for existing hyperlinks.
- If you want to use the URL Builder window to modify a hyperlink, you can recreate the hyperlink and include your modifications in the URL Builder window.
. Then, in the drop-down list, select either one or both of the
button.
.