Manage Data Permissions
View Existing Data Permissions
Grant Data Permissions
Procedure
About Entity Family Data Permissions
For each entity family, you can grant users View, Update, Insert, and Delete permissions. The following table provides details about each permission.
| Permission | Description | Notes |
|---|---|---|
| View | Users can view records that belong to the family. Users with only View permissions on a family will be able to open existing records belonging to that family but would not be able to create, modify, or delete them. |
For typical users, View permissions are a prerequisite to Update, Insert, and Delete permissions because they provide users with the initial access required for modify, create, and delete operations. For example, users with View permissions on a family can:
|
| Update | Users can modify records that belong to the family. Users with only Update permissions on a family would be able to modify existing records belonging to that family but would not be able to view, delete, or create records in that family. | Typically, you would not grant Update-only permissions to a user because, while that user would be able to modify records in that family, without View permissions, they would not be able to search for them or open them. Update-only permissions, however, may be used to support processes and operations that occur outside of the user interface (i.e., interfaces or scheduled jobs). |
| Insert | Users can create records in the family. Users with only Insert permissions on a family would be able to create records in that family, but would not be able to view, modify, or delete them. | Typically, you would not grant Insert-only permissions to a user because, while that user would be able to create records in that family, without View permissions, they would not be able to initiate the record-creation process in APM. Insert-only permissions, however, may be used to support processes and operations that occur outside of the user interface (i.e., interfaces or scheduled jobs). |
| Delete | Users can delete records that belong to the family. Users with only Delete permissions on a family would be able to delete records belonging to a family, but would not be able to view, modify or create them. | Typically, you would not grant Delete-only permissions to a user because, while that user would be able to delete records in that family, without View permissions, they would not be able to perform a search to find the records that they wanted to delete. Delete-only permissions, however, may be used to support processes and operations that occur outside of the user interface (i.e., interfaces or scheduled jobs). |
About Relationship Family Data Permissions
Relationship family permissions are similar to entity family permissions in that the same permission levels are available: View, Update, Insert, and Delete. Each permission level, however, provides access that is slightly different from the access provided through entity family permissions.
Remember that relationship families are used to create links between records in entity families. Consider an example where the Equipment family is related to the Failure family through the Has Failure relationship. In this case, to provide a user with full access to an Equipment record and its associated Failure record, that user would need permissions to three families: Equipment, Failure, and Has Failure.
The following table provides details about each relationship family data permission.
| Permission | Description | Notes |
|---|---|---|
| View | Users have basic access to the links that relate predecessor and successor records. Users with View-only access to a relationship family can open existing linked records, but cannot link and unlink records using that relationship. |
None |
| Update | Users can modify existing links in a relationship family. | This applies only in cases where fields are defined for the relationship family. Users with Update permissions will also need View permissions. |
| Insert | Users can link records together using that relationship family. Using the previous example, a user would need Insert permissions on the Has Failure family to link Equipment records to Failure records. | Users with Insert permissions will also need View permissions. |
| Delete | Users can unlink records associated with the relationship family. Using the previous example, a user would need Delete permissions on the Has Failure family to unlink Failure records from Equipment records. | Users with Delete permissions will also need View permissions. |
.
.
.