Amplification Codes
Access an Amplification Code
Procedure
- Access the GAA Administrator page.
- In the System Codes section, select Amplification Codes.
The Amplification Codes subsection appears, displaying the following columns of information:
- Amplification Code
- Code Description
- Unit Type
- Event Type
- Regulatory Organization
- Locate the row that contains the Amplification Code that you want to access.
- In the Amplification Code column, select the link.
The Edit Amplification Code window appears, displaying the datasheet of the selected Amplification Code.
Note: As needed, you can modify the values in the available fields, and then select
to save your changes.
Add an Amplification Code
Procedure
- Access the GAA Administrator page.
- In the System Codes subsection, select Amplification Codes.
The Amplification Codes section appears.
- In the upper-left corner of the Amplification Codes section, select
.The Add Amplification Code window appears.
- As needed, enter the values in the available fields.
- Select
.The new Amplification Code is added.
Delete an Amplification Code
About This Task
Important: You must not delete a baseline Amplification Code.
Procedure
- Access the GAA Administrator page.
- In the System Codes subsection, select Amplification Codes.
The Amplification Codes section appears.
- Select the row containing the Amplification Code that you want to delete.
- In the upper-right corner of the Amplification Codes section, select
.
The Delete Amplification Code dialog box appears, asking you to confirm that you want to delete the selected Event Type.
- Select Yes.
The selected Amplification Code is deleted and the updated list of Amplification Codes appears.