Generation Availability Analysis Wind
Deploy GAA Wind for the First Time
Before You Begin
The following table outlines the steps that you must complete to deploy and configure this module for the first time. These instructions assume that you have completed the steps for deploying the basic system architecture.
These tasks may be completed by multiple people in your organization. GE Digital recommends, however, that the tasks be completed in the order in which they are listed.
Results
Step | Task | Notes |
---|---|---|
1 |
Review the GAA Wind data model to determine which relationship definitions you will need to modify to include your custom equipment and location families. Via Configuration Manager, modify the relationship definitions as needed. |
This step is required only if you store equipment and location information in families other than the baseline Equipment and Functional Location families. |
2 | Assign Security Users to one or more of the GAA Wind Security Groups and Roles. | This step is required. |
3 | Specify additional system code tables for the GAA Wind families. | By default, GE Digital APM provides a set of system code tables for the GAA Wind families. You can modify these default system code tables or add new system code tables. |
4 | Configure the GAA Wind Report Configuration records. | This step is required. |
5 | Using the GAA Wind Asset Hierarchy Data Loader, create the following records in the GAA Wind Asset Hierarchy:
| This step is required. |
6 | Using the GAA Wind Sub Group Capacity Data Loader, create the GAA Wind Sub Group Capacity record. | This step is required. |
Upgrade or Update GAA Wind to V4.6.8.0.0
Before You Begin
The following tables outline the steps that you must complete to upgrade this module to V4.6.8.0.0. These instructions assume that you have completed the steps for upgrading the basic GE Digital APM system architecture.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.