GE Digital APM Client
Hardware Requirements
The following hardware requirements outline the minimum hardware required for any machine or mobile device that will access the GE Digital APM system. These requirements account for the GE Digital APM software only. Additional hardware may be required on clients where other components are installed. These requirements may not be sufficient, depending upon how your system is configured.
Desktops and Laptops
| Minimum Requirements | Recommended Requirements for Optimal User Experience |
|---|---|
| Two Processor Cores, 2 GHz | Six Processor Cores, 2.6 GHz (for example, Intel Core i7 9750 H- High performance CPU |
| 4 GB RAM (8 GB RAM recommended) | 32 GB RAM |
| 8 GB of available hard drive space | 512 GB Solid State Drive |
| 13" screen | Graphics Card with 4GB of RAM (for example, Nvidia Quadro series) |
| 1024 X 768 screen resolution | 1920 X 1080 screen resolution |
Mobile Devices
You can use GE Digital APM on mobile devices either in the GE Digital APM mobile application or in the web browser on the device. The following information is generic and pertains to using the application on mobile devices in either of these scenarios. For specific information regarding the mobile application, see the GE Digital APM Mobile Application portion of the Getting Started section of this documentation.
Support for mobile devices is provided in two resolution view modes: full or limited. Full-resolution view mode supports access to the entire GE Digital APM system. Limited-resolution view mode supports limited access to overview pages and data collection. Resolution view mode is determined by the type of device that is used to access GE Digital APM, and is not a selectable option.
| Minimum Requirements | Devices Tested |
|---|---|
|
Minimum requirements for full-resolution view mode:
|
Devices used in the GE Digital APM testing environment:
|
|
Minimum requirements for limited-resolution view mode:
|
Devices used in the GE Digital APM testing environment:
|
Small Screen Devices
| Minimum Requirements | Devices Tested |
|---|---|
|
Minimum requirements:
|
Devices used in the GE Digital APM testing environment:
|
Software Requirements
The following software components are required on any machine or device that will access the GE Digital APM system using a browser. If the software meets the following requirements, you can access GE Digital APM using any operating system.
One of the following browsers is required for desktops, laptops, and mobile devices:
| Browser | Notes |
|---|---|
| Latest version of Google Chrome |
|
| Microsoft Edge |
New versions of Microsoft Edge are released every 4 weeks. Each version includes security updates, new features, and possible breaking changes. To ensure compatibility, GE Digital recommends that you use the latest Microsoft Edge version available. |
- You can access GE Digital APM via the browser on a mobile device, but it is recommended that you install and use the GE Digital APM mobile application for an enhanced experience. On a mobile device, to ensure that the mobile application works as intended, you should set your default browser to the desktop versions of Chrome or Internet Explorer (as opposed to the application versions).
- The method used to access Reference Documents in the GE Digital APM mobile application will vary depending on your device platform. For example, on Windows and Android devices, the first time you access Reference Documents, you will be prompted to select the application in which you want to open a file, and this selection will then become the default. Apple iOS will always prompt you to select an application. On all platforms, you will also be prompted when the platform for your device does not recognize the file type that it is attempting to download.