Health Indicator Source Management
About Health Indicator Source Management
In Health Indicator Source Management, you can indicate which health indicator source records should be monitored by Asset Health Manager. If a source record is excluded, AHM will ignore data related to that source when processing health information for an asset.
About Automatic Creation of Health Indicators
After you start the Asset Health Indicator service, whenever an entity or a relationship record is created in the APM database, Health Indicator records are created automatically if the following conditions are met:
- A valid health indicator source record exists (i.e., a record belonging to a family that with a fully configured Health Indicator Mapping record).
- The health indicator source record is linked to an asset record (that is, a record in a family that is included in the Asset Hierarchy definition) and the Has Health Indicators relationship definition exists for that asset family.
- A Health Indicator record does not already exist for the health indicator source record and the asset record.
- The health indicator source record is included in the Health Indicator Source Management workspace.
- For Measurement Location health indicator source records, the Include as Health Indicator Source check box on the data sheet is selected.
Records may exist in your database that belong to a health indicator source family, but for which you do not want health indicators to be created. You can use the Health Indicator Source Management workspace to manage whether health indicators are created for each potential source record.
When Health Indicator records are created:
- The asset record will be linked to the newly created Health Indicator record(s) through the Has Health Indicators relationship.
- The Health Indicator record(s) will be linked to the corresponding health indicator source and Health Indicator Mapping records according to the AHM data model.
- If reading data (from health indicator reading source records) is available, the initial status of the health indicator will be set accordingly.
Once Health Indicator records exist in the APM database, you can view the related health information in Asset Health Manager.
If a health indicator source record is deleted or if it is unlinked from an asset record to which it was linked through the relationship defined in the relevant Health Indicator Mapping record, the corresponding Health Indicator records are deleted automatically.
Health Indicators and Site Filtering
When a health indicator source record is linked to an asset, both the health indicator source record and the newly created Health Indicator record inherit the Site Reference Key of the asset.
In certain scenarios, you may be working with a health indicator source that measures some values that are shared across sites. For example, you may have a Measurement Location that measures flow or pressure in a pipe that crosses a site boundary. In this case, the health indicator source (e.g., Measurement Location record) should be designated as a global record (that is, not assigned to any specific site). Because health indicator source records automatically inherit the Site Reference Key of the asset, after linking the source to the asset, a Super User must use the Site control to adjust the site assignment of the source records to designate them as Global.
Include or Exclude Sources from Automatic Health Indicator Creation
About This Task
Procedure
View the Time Stamp of the Last Health Indicator Update
In the AHM Admin page, you can determine whether your Health Service is running by viewing the time stamp of the most recently updated health indicator source. If the date and time displayed seem older than you expect, you may need to take further steps to confirm whether your Health Service is functioning as expected.
Procedure
Resync Health Indicators
If the list of health indicator sources in the AHM Admin page becomes out of sync with the actual list of available health indicators, an admin may need to resync your health indicators.
to search for a source record matching a keyword in any column. If you search in the
to filter the grid to show only the source records in specific families.