Reference

APM Connect System Requirements

License Requirements

APM Connect has a three-tier license system that enables the APM Connect Framework. One of the following license types is required to take advantage of the APM Connect functionality:

  • APM Connect Basic
  • APM Connect Plus
  • APM Connect Studio
    Note: APM Connect Studio contains numerous libraries that integrate with third-party products, such as GeoRaster. Questions regarding linking these libraries with APM should be directed to a member of the APM Professional Services department on an individual basis. Specific requirements of third-party products is outside the scope of APM Connect Studio support.

Additional Licensing

The following additional licenses are required to take advantage of various Adapters:

AdapterLicenseDescription
SAP AdapterSAP Integration InterfacesEnables the SAP Equipment, Functional Location, Work History, and Notification Creation Adapters.
SAP Technical CharacteristicsEnables the SAP Technical Characteristics Adapter.
SAP Work ManagementEnables the SAP Work Management Adapter.
SAP PI AdaptersSAP Process IntegrationEnables the SAP PI Adapters.
Maximo AdaptersMaximo InterfacesEnables the Maximo Equipment, Functional Location, Work History, Service Request, and Work Order Generation Adapters.
Note: There is no additional license required to take advantage of the APM Connect Data Loader functionality.

UDLP Versions

Beginning with the Sept. 21, 2018 release, APM will maintain compatibility with the APM Connect client-side jobs one version prior to the newly released version.

To prevent processing failures, you must upgrade your on-premises, client-side jobs within two months of a APM release to the most current version of the APM Connect client jobs. For example, if the APM tenant has installed the Dec. 14, 2018 release, you must upgrade the on-premises, client-side jobs to UDLP V2.5.0 or V2.5.1 by Feb. 14, 2019, otherwise the next release of the APM tenant may not process your data correctly.

The following UDLP versions are currently supported in APM:

  • V2.9.0

Additional Components Required for APM Connect

In addition to the basic APM system architecture, your system must also contain the following components:

Minimum Software Requirements
  • Windows Server 2012
  • Windows Server 2016
  • Open JDK 11

Recommended Software for APM Connect Server

  • Windows Server 2016 R2

Browser Requirements for APM Connect Server

Web BrowserRecommended or Supported
Mozilla Firefox ESR 68Supported
Mozilla Firefox up to latest available browser versionSupported
Microsoft Internet Explorer 11 or laterSupported
Microsoft Edge up to latest available browser versionSupported
Apple Safari 12 or laterSupported
Google Chrome up to latest available browser versionRecommended

Minimum Hardware Requirements for APM Connect Server

  • Four Processor Core, 2.0GHz
  • 16 GB RAM
  • 100 GB Free Disk
  • 100 MB Network Interface

Recommended Hardware for APM Connect Server

  • I5 Processor, 2.0 + GHz
  • 32 GB RAM
  • 300 GB Free Disk
  • 1 GB Network Interface
Tip: APM Connect is input and output intensive, and requires a large amount of storage space. Faster storage is the best way to improve the performance of APM Connect.

Depending on how your system is configured, these requirements may not be sufficient. Parameters that affect the hardware requirements include the number of users, modules purchased, database size, and other factors that can vary from one customer to another. For help refining your specific system requirements, contact GE Vernova

System Architecture for EAM Adapters

Figure: Single Server Configuration (Recommended)

The single server configuration is the simplest way to configure APM Connect. However, it does include an embedded database. The following image depicts this configuration.

Figure: External Database Configuration

Many organizations choose to separate their databases. It is possible to install the intermediate repository database on an external server, and to keep the APM Connect Systems database on a different server. The following image depicts this configuration.

Note: The external configuration will affect performance. The single server configuration results in faster performance.

Deploying APM Connect

After you have installed and configured the basic APM system architecture, you will need to perform some configuration steps specifically for APM Connect.

Note: You need to perform this process only if you are using an EAM Adapter or a Field Service system Adapter.

Required Server Ports

To provide communication between APM Connect and other systems, make sure the listed ports are open.

Port NumbersDescription
80, 9080, 8879, 9043, 9044, 9060, 9061, 9430, 9443, 139, 50000, 50005, 3300Used for SAP and Maximo Interfaces.
8080, 8005, 7000, 7001, 7777, 7555,1099, 8040, 8101, 9001, 44444, 5432Used for APM Interfaces.
  • 6220 - Dedicated
  • 7220 - RAC
Used for the Oracle client.

APM Connect Version Compatibility Table

This topic provides the installation files that are required for an APM Connect installation, and the version structure for APM Connect.

APM Compatibility Table

This table includes only the APM versions for which a corresponding APM Connect version was released.

APM Framework VersionAPM Connect BaseData LoaderEAM MaximoEAM SAPEAM SAP CloudEAM SAP PI
V4.6.9.0.0APM Connect Base V3.0.2 - PatchUDLP V3.5.0 or V3.4.0
V4.6.8.0.0APM Connect Base V3.0.2 - PatchUDLP V3.5.0 or V3.4.0
V4.6.7.0.0APM Connect Base V3.0.2 - PatchUDLP V3.5.0 or V3.4.0
V4.6.6.0.0APM Connect Base V3.0.2 - PatchUDLP V3.5.0 or V3.4.0
V4.6.5.0.0APM Connect Base V3.0.3UDLP V3.4.0 or V3.3.0
V4.6.4.0.0APM Connect Base V3.0.2UDLP V3.3.0 or V2.9.0
V4.6.3.0.0APM Connect Base V3.0.2UDLP V3.3.0 or V2.9.0
V4.6.2.0.0APM Connect Base V3.0.2UDLP V3.3.0 or V2.9.0
V4.6.1.0.0APM Connect Base V3.0.0UDLP V3.2.0 or V2.9.0
V4.6.0.0.0 (December 17, 2021)APM Connect Base V3.0.0UDLP V3.1.0 or V2.9.0
V4.5.0.0 (September 29, 2020)APM Connect Base V2.0.0UDLP V2.9.0 or V2.8.0
V4.4.0.0 (April 28, 2020)APM Connect Base V2.0.0UDLP V2.8.0, V2.7.0, or V2.7.1
V4.3.1.0.1 (October 29, 2019)APM Connect Base V2.0.0UDLP V2.7.0, V2.7.1, V2.6.0, or V2.6.1
Note: UDLP V2.7.0 and V2.7.1 are identical for Cloud Server revision only.
V4.3.1.0.0 (September 17, 2019)APM Connect Base V2.0.0UDLP V2.6.0 or V2.6.1 and V2.7.0
V4.3.0.7.5 (June 19, 2019)APM Connect Base V2.0.0UDLP V2.5.0 or V2.5.1 and V2.6.0 or V2.6.1
V4.3.0.7.0 (March 29, 2019) APM Connect Base V2.0.0UDLP V2.5.0 or V2.5.1 and V2.6.0
V4.3.0.6.5 (December 7, 2018 APM Connect Base V2.0.0UDLP V2.4.0 and V2.5.0 or V2.5.1
V4.3.0.6.0 (September 21, 2018) APM Connect Base V2.0.0UDLP V2.4.0 and V2.5.0
V4.3.0.5.0 (June 22, 2018) APM Connect Base V2.0.0UDLP V2.4.0
V4.3.0.4.0 (April 25, 2018) APM Connect Base V2.0.0 UDLP V2.3.0
V4.3.0.3.0 (December 11, 2017)APM Connect Base V2.0.0UDLP V2.2.0EAM SAP PI V2.0.0
V4.3.0.2.0 (September 22, 2017)APM Connect Base V2.00UDLP V2.1.0EAM MAX V2.0.0UDLP V2.1.0EAM SAP PI V2.0.0
V4.3.0.1.0 (August 16, 2017)APM Connect Base V2.00DL V2.0.1EAM MAX V2.0.0EAM SAP V2.0.0EAM SAP Cloud V1.0.1EAM SAP PI V2.0.0
V4.3.0.0.0 (June 30, 2017)APM Connect Base V2.00DL V2.0.0EAM MAX V2.0.0EAM SAP V2.0.0EAM SAP Cloud V1.0.1EAM SAP PI V2.0.0
V4.2.0.6.0 (March 21, 2017)APM Connect Base V1.0.3DL V1.6.3EAM MAX V1.1.2EAM SAP V1.6.3EAM SAP Cloud V1.0.1EAM SAP PI V1.1.2
V4.2.0.4.0 (December 13, 2016)APM Connect Base V1.0.3DL V1.6.3EAM MAX V1.1.2EAM SAP V1.6.3EAM SAP Cloud V1.0.1EAM SAP PI V1.1.1
V4.2.0.3.0 (November 15, 2016)APM Connect Base V1.0.3DL V1.6.3EAM MAX V1.1.0EAM SAP V1.6.3EAM SAP Cloud V1.0.1EAM SAP V1.1.1
V4.2.0.2.0 (October 17, 2016)APM Connect Base V1.0.3DL V1.6.2EAM MAX V1.1.0EAM SAP V1.6.2EAM SAP Cloud V1.0.1EAM SAP V1.1.1
V4.2.0.1.0 (September 21, 2016)APM Connect Base V1.0.3DL V1.6.2EAM MAX V1.1.0EAM SAP V1.6.1EAM SAP Cloud V1.0.0EAM SAP V1.1.1
V4.2.0.0 (July 27, 2016)APM Connect Base V1.0.3DL V1.6.1EAM MAX V1.1.0EAM SAP V1.6.1EAM SAP Cloud V1.0.0EAM SAP PI V1.1.1
V4.1.7.0 (June 6, 2016)APM Connect Base V1.0.2DL V1.6.0EAM MAX V1.1.0EAM SAP V1.6.0N/AEAM SAP PI V1.1.0
V4.1.6.3 (June 20, 2016)APM Connect Base V1.0.2DL V1.5.6EAM MAX V1.0.0EAM SAP V1.5.5N/AEAM SAP PI V1.0.1
V4.1.6.2 (May 20, 2016)APM Connect Base V1.0.2DL V1.5.5EAM MAX V1.0.0EAM SAP V1.5.5N/AEAM SAP PI V1.0.1
V4.1.6.0 (March 28, 2016)APM Connect Base V1.0.2DL V1.5.4EAM MAX V1.0.0EAM SAP V1.5.5N/AEAM SAP PI V1.0.1
V4.1.5.1 (March 11, 2016)APM Connect Base V1.0.2DL V1.5.3EAM MAX V1.0.0EAM SAP V1.5.3N/AEAM SAP PI V1.0.0
V4.1.5.0 (February 9, 2016)APM Connect Base V1.0.2DL V1.5.2EAM MAX V1.0.0EAM SAP V1.5.3N/AEAM SAP PI V1.0.0
V4.1.1.1 (December 15, 2015)APM Connect Base V1.0.2DLV1.5.1N/AEAM SAP V1.5.2N/AEAM SAP PI V1.0.0
V4.1.1.0 (November 23, 2015)APM Connect Base V1.0.2DL V1.5.0N/AEAM SAP V1.5.2N/AEAM SAP PI V1.0.0
V4.1.0.3 (March 7, 2016)APM Connect Base V1.0.2DL V1.4.1N/AEAM SAP V1.5.1N/AEAM SAP PI V1.0.0
V4.1.0.0 (October 12, 2015)APM Connect Base V1.0.2DL V1.4.0N/AEAM SAP V1.5.1N/AEAM SAP PI V1.0.0
V4.0.0.0 (July 23, 2015)APM Connect Base V1.0.2WPA V1.2.1N/AEAM SAP V1.5.0N/AEAM SAP PI V1.0.0

The Automatic Data Loader Directories

The automatic data loader job uses directories within the directory identified in the SCAN_DIR parameter to identify the data loader to use for a particular workbook.

Data Loaders and Directories

The following table lists the directories that are created when the job starts that correspond to the various data loaders.
Data Loader NameDirectory Name
APM FamilyManageAPM
Asset Criticality Analysis (ACA)ACADataLoader
Asset Criticality Analysis (ACA Checklist)ACACheckListDataLoader
Asset Ingestion LoaderAssetIngestionLoader
Asset Strategy Management (ASM)ManageASM
Asset Strategy Management (ASM) TemplatesManageAssetStrategyTemplate
CalibrationCalibration Loader
Custom Asset HierarchyCustom Asset Hierarchy Loader
Equipment and Functional LocationManageEquipmentAndFunctionalLocation
Failure Modes and Effects Analysis (FMEA)ManageRCMFMEA
Failure Modes and Effects Analysis (FMEA) Analysis TemplatesManageFMEAAnalysisTemplate
Failure Modes and Effects Analysis (FMEA) Asset TemplatesManageFMEAAssetTemplate
Generation Availability Analysis (GAA) Amplification CodesGAA GADS Amplification Code
Generation Availability Analysis (GAA) Cause CodeGAA GADS Cause Code
Generation Availability Analysis (GAA) EventsGAA Events
GAA Wind Asset HierarchyGAA Wind Asset Hierarchy
GAA Wind EventsGAA Wind Events
GAA Wind Sub Group CapacityGAA Wind Sub Group Capacity
Geographic Information System (GIS)GISDataLoader
HazardsHazards Loader
Inspection Management (IM) AssetsManageInspections
Inspection Management (IM) Functional LocationManageInspectionsFL
Production Loss Analysis (PLA) AdminPLA Admin Data
Production Loss Analysis (PLA) PlanPLA Plan Data
Production Loss Analysis (PLA) Production EventProduction Event Data
Reliability Centered Maintenance (RCM)ManageRCM
RCM Analysis TemplateManageRCMAnalysisTemplate
Risk Based Inspection (RBI) 580ManageRBI580
Risk Based Inspection (RBI) 581ManageRBI581
Risk Based Inspection (RBI) Corrosion LoopLoad RBI Corrosion Loop
Risk MatrixRiskMatrixDataLoader
RoleRoleDataLoader
Root Cause Analysis (RCA)Manage RCA
Rounds Allowable ValuesRounds Allowable Value
Rounds ReadingsRounds Readings
Rounds RoutesRounds Route
Rounds TemplatesRounds MLTG
Tags to Assets RelationshipManageTagLinks
TaxonomyManageTaxonomy
Thickness Monitoring (TM) EquipmentManageTMLGroup
Thickness Monitoring (TM) Functional LocationManageTMLGroupFL
Work HistoryManageWorkHistory