Mouse Up Event
Mouse Up triggers a procedure or calls a script when the left mouse button is clicked then released.
Note: This event also occurs when a user releases the Enter key on the keyboard.
| Field | Description | ||||||
|---|---|---|---|---|---|---|---|
| A | Action | Contains a drop-down list of existing procedures and scripts. Use either of the following. | |||||
| Procedure | |||||||
| Script | |||||||
| B | Parameter | Can be used if the event invokes a script directly or through a procedure parameters are: The default code begins as follows. Sub OnMouseUp(x As Long, y As Long, flags As Long) Where parameters are | |||||
| x | |||||||
| y | |||||||
| flags | |||||||
| C | Debounce event | Check | |||||
| Clear | |||||||
|
Note: When debouncing is enabled, the event/action queue is always processed one action at a time; the current action must be completed before the next action can start.
This makes the queue's event/action sequencing predictable and avoids situations where many events could trigger actions and consume unacceptable levels of CPU and memory.
|
|||||||