Data Sources
About Advanced Visualization Data Sources
Advanced Visualization provides out of the box capabilities that enable you to visualize data for the following APM features and modules:
- Alerts
- Analytics
- Assets
- Baseline entities and queries
- Cases
- Cost Benefit Analysis (CBA)
- General recommendations
- SmartSignal
- Time Series Data
Each of these features is associated with a set of data sources in Advanced Visualization. The data sources contain a set of logically related fields that allow you to create and customize the visualizations based on the access privileges that you have for the specific feature.
Note: Although you have access to all the data sources, you must also have access to the required capabilities to create visualizations using these data sources. You can visualize the data for the assets based on the permissions granted to your APM user account.
The following table provides high-level information about the data sources available for the supported modules or features:
Module/Feature | Data Source Description |
---|---|
Alerts | You can visualize data using one of the following types of business views available in the APM baseline domain:
Note:
|
Analytics | You can visualize analytic data using one of the following types of business views available in the APM baseline domain:
Note: You cannot modify the baseline business view. However, you can create a copy of the view that you want to modify within your tenant, and then modify the view as needed.
|
Assets | You can visualize assets data using one of the following types of business views available in the APM baseline domain:
Note: You cannot modify the baseline business view. However, you can create a copy of the view that you want to modify within your tenant, and then modify the view as needed.
|
Cases | You can visualize data using one of the following types of business views available in the APM baseline domain:
Note:
|
CBA | You can visualize data using one of the following types of business views available in the APM baseline domain:
Note: You cannot modify the baseline business view. However, you can create a copy of the view that you want to modify within your tenant, and then modify the view as needed. |
General Recommendations | You can visualize data based on the general recommendations data available within APM. Note: In Legacy Predix APM, you cannot create visualizations based on this data source as no date will be available for you in the data source. |
APM Baseline Entities | You can visualize data using the baseline entity views available in APM. Note:
|
APM Baseline Queries | You can visualize data using the baseline query views available in APM. Note:
|
SmartSignal | You can visualize SmartSignal analytic models using one of the following types of business views available in the APM baseline domain:
Note:
|
Time Series Data | You can visualize time series data that is collected for a set of asset tags associated with your tenant. The data source is created based on a reporting object and curated for creating customized visualizations. |
Create a Data Source using an APM Query
Before You Begin
- Make sure that the baseline query or the custom query that you want to use to create a data source exists in the Catalog.
About This Task
This topic describes how to create a data source using a baseline query or a custom query, and configure the data source to enable the Advanced Visualization users to create charts or dashboards using the data source.
Procedure
What To Do Next
Retrieve Query Details of a APM Query using Query Helper
About This Task
When creating a data source using a baseline or custom query, you must have the following query details:
- Sample request body for the Insert (POST) operation
- Service URL extension
- Valid query path
- Valid query parameters and parameter values
This task describes how to retrieve and validate the parameter details of a query to create a data source.