Asset Health Manager Deployment
Deploy AHM for the First Time
The following table outlines the steps that you must complete to deploy and configure this module for the first time.
These tasks may be completed by multiple people in your organization. We recommend, however, that the tasks be completed in the order in which they are listed.
Before you begin completing these tasks, review the system requirements for this module to identify the supported features for this module in APM.
Step | Task | Notes |
---|---|---|
1 | Assign Security Users to one or more of the Asset Health Manager Security Roles. | This step is required. |
2 |
Determine the equipment or location whose overall health you want to evaluate, and make sure that an asset record exists in the database for this equipment or location and is included in the Asset Hierarchy configuration. |
This step is required. |
3 | Configure Health Indicator Mapping records for each family that you want to use as a health indicator source, for which a baseline Health Indicator Mapping record does not already exist. |
This step is required. Baseline Health Indicator Mapping records exist for the following health indicator source families:
|
4 | Link each asset record to the record(s) that you want to use as a health indicator source records. | This step is required. |
5 | For any specific records in a health indicator source family for which you do not want health indicators to be created, exclude these records from the automatic health indicator creation. | This step is optional. |
6 | Review the baseline event mappings and modify or create new mappings as necessary to customize the information that is displayed in the Events section in Asset Health Manager. | This step is optional. Refer to the Asset Health Manager end user help for more information about events. |
AHM Security Groups
The following table lists the baseline Security Groups available for users within this module, the baseline Roles to which those Security Groups are assigned, and the OT Connect groups that are assigned to the Health Roles to support the Health and OT Connect integration. In Cloud APM, Roles are assigned to Security Users through permission sets.
Security Group | Roles |
---|---|
MI AHI Administrator | MI Health Admin MI Strategy Admin MI Strategy Power |
MI AHI User | MI Health Power MI Health User MI Strategy Admin MI Strategy Power MI Strategy User |
MI AHI Viewer | None |
MI OT Connect Administrator MI OT Connect User | MI Health Admin |
MI OT Connect Viewer MI Content Template Viewer | MI Health Power MI Health User |
The baseline family-level privileges that exist for these AHM Security Groups are summarized in the following table.
Family | MI AHI Administrator | MI AHI User | MI AHI Viewer |
---|---|---|---|
Entity Families | |||
Checkpoint Task | View, Update, Insert | View, Update, Insert | View |
Event Mapping | View, Update, Insert, Delete | View | View |
Health Indicator | View, Update, Insert, Delete | View, Update | View |
Health Indicator Mapping | View, Update, Insert, Delete | View | View |
Health Indicator Value | View, Update, Insert, Delete | View | View |
KPI | View | View | View |
KPI Measurement | View | View | View |
Measurement Location | View | View | View |
Measurement Location Template | View | View | View |
OPC Reading Note: This family is obsolete from the March 27, 2020 release. | View | View | View |
OPC System Note: This family is obsolete from the March 27, 2020 release. | View | View | View |
OPC Tag Note: This family is obsolete from the March 27, 2020 release. | View | View | View |
Operator Rounds Allowable Values | View | View | View |
Policy | View | View | View |
Policy Event | View, Update, Insert, Delete | View, Update, Insert, Delete | View |
Policy Instance | View | View | View |
Reading | View | View | View |
Recommendation | View, Update, Insert, Delete | View, Update, Insert, Delete | View |
Timestamped Value | View, Update, Insert, Delete | View | View |
Relationship Families | |||
Has Checkpoint | View | View | View |
Has Child Hierarchy Item (Deprecated) | View, Update, Insert, Delete | View | View |
Has Consolidated Events | View, Update, Insert, Delete | View, Update, Insert, Delete | View |
Has Health Indicators | View, Update, Insert, Delete | View | View |
Has OPC Reading Note: This family is obsolete from the March 27, 2020 release. | View | View | View |
Has OPC Tag Note: This family is obsolete from the March 27, 2020 release. | View | View | View |
Has Readings | View | View | View |
Has Recommendations | View, Update, Insert, Delete | View, Update, Insert, Delete | View |
Has Timestamped Value | View, Update, Insert, Delete | View | View |
Health Indicator Has Mapping | View, Update, Insert, Delete | View | View |
Health Indicator Has Source | View, Update, Insert, Delete | View | View |