Analytic Templates
About Analytics Templates
In this section, you will learn about analytic templates and the analytic catalog. Analytics generate data to help you manage your assets. Application Analytics enables you to build analytic templates and upload analytics to the analytic catalog.
Analytics implement mathematical models to provide intelligence about your assets, helping you manage them more efficiently. For example, you can use analytics to trigger alerts, generate maintenance advisories, and produce performance statistics.
Application Analytics enables you to create an analytic template that you can use in multiple deployments for the specified runtime. By employing a template, you can reuse the same analytic to deploy to different assets using asset applicability, and create unique input-output (I/O) tag mapping per deployment. You can also vary the schedule per deployment. The framework expects unique name per deployment.
The analytic catalog groups the tasks necessary to successfully configure and deploy an analytic.
Add an Analytic Template
Add the analytic packaged implementation to the Application analytic catalog to be deployed to a specific analytic runtime for running the analytic.
Before You Begin
Be sure that the packaged implementation containing the code for your analytic and any supporting files, such as instructions for deployment, are available to upload.
About This Task
The system validates the Name and Analytic File fields before you can proceed. You will need to enter or select values based on the selected runtime type.
Depending on the type of analytic implementation the configuration options vary for adding the template to the catalog. The analytic runtime environments supported for your tenant vary based on the tenant configuration.
Procedure
- In the Applications menu, navigate to .
- Select
in the page heading.
- Add the analytic template using one of the following methods:
- Select the Import from file box. To ingest the complete analytic template, you must have the valid analytics ingestion .zip file ready. Refer to the topic Understand Analytic Ingestion in the reference section.
- Select Submit.
Results
The template is saved to the catalog. After the analytic logic is successfully uploaded, the status changes to Published.
What To Do Next
Analytic Template Fields based on Runtime
List of analytic template configuration requirements for different runtimes.
Field Requirements Based On Runtime
Refer to the table below to see the required and optional data entry fields based on the selected analytic runtime for the analytic template. Availability of a specific runtime is dependent on the tenant configuration.
Field Name | Description | GEDCR | SmartSignal | Power Fabric |
---|---|---|---|---|
Data Frame Types | This value determines the way the Application Analytics expects the input.json file format for the analytic algorithm. It also determines the format in which Application Analytics creates the corresponding output.json and PortToField.json files. |
| N/A | N/A |
Name | A unique name for the analytic template. | Required | Required | Required |
Owner | The name of the analytic owner, typically the developer of the analytic logic. | Required | Required | Required |
Analytic Type | The language used to develop the analytic. |
| Smartsignal | CCAP (Version: 3.1) |
Type Version | The version for the selected language. The type version is updated based on the analytic type selected. | Required | Required | As defined in the runtime configuration |
Analytic File | Select ![]() Note: The uploaded file must be in .zip or .jar format. | Required | Required | Required |
Analytic Version | Version of the uploaded analytic implementation. | Required | Required | Required |
Analytic Version Update | The information specific to what is new or changed in this version of the uploaded analytic package. | Optional | Optional | Optional |
Primary Category | The main category tag used for the analytic. This tag allows the analytic to be classified under the designated category for further discovery in the catalog. Enter a value that best matches the type of analytic you are creating. For example, if monitoring a turbine, you can select Monitoring. | Required | Required | As defined in the runtime configuration |
Secondary Category | The secondary category tag used for the analytic. This tag allows the analytic to be classified under the designated category, allowing you to further refine where the analytic is applied. | Optional | Optional | As defined in the runtime configuration |
Enable Template Export | Your packaged Analytics Template will be available for download once template is publish successfully. | Required | N/A | N/A |
You can configure these settings using the user interface or the AnalyticDefinition.json file (as shown in the following section) depending on the runtime. The AnalyticDefinition.json file is included in the analytic ingestion package (.zip file) that is imported during template creation. For GEDCR runtime, however, you can configure these settings only using the AnalyticDefinition.json file.
Sample AnalyticDefinition.json File
{
"@type": "analyticEntryPxMetaData",
"contractVersion": "1.0.0",
"initNameSuffix": false,
"name": "threshold",
"author": "Support team from ingestion",
"description": "APM threshold from ingestion with attribute constant",
"runtimeName": "GEDCR",
"primaryCategory": "Monitoring",
"secondaryCategory": "",
"hasAnalyticArtifact": true,
"analyticVersion": "1.0.0",
"templateDownloadEnabled" : true,
"analyticRecipientEmails":["test@ge.com"],
"keyValueStore": {
"runtimeTemplateId": "",
"runtimeTemplateName": "",
"runtimeTemplateVersion": ""
},
"customInputSupported": false,
"customConstantSupported": false,
"customOutputSupported": false,
"analyticArtifact": {
"hashCode": 0,
"uri": "",
"name": "../executableFile/threshold-analytic-python-alerts.zip",
"description": "",
"filename": "../executableFile/threshold-analytic-python-alerts.zip",
"version": "",
"artifactType": "",
"contentLength": 0,
"metaData": {},
"pxAnalyticId": "",
"keyValueStore": {},
"language": "Python",
"languageVersion": "3.5",
"isDirty": false
},
"analyticDefine": {
"@type": "analyticDefinePx",
"supportingFiles": [],
"inputs": [
{
"@type": "analyticInput",
"hashCode": 0,
"uri": "/ports/abbe2ef0-0d32-4819-83cf-fc11f8668f2e",
"name": "temperature",
"description": "Any Temperature Tag is sufficient here to make a point",
"dataType": "Double",
"unit": "Fahrenheit",
"unitGroup": "",
"dataSourceType": "APM_TIMESERIES",
"mappingValueType": "TAGS",
"isVariablePort": false,
"isRequired": false,
"isDirty": false
},
{
"@type": "analyticInput",
"hashCode": 0,
"uri": "/ports/7bc0ce36-598e-4655-8935-10b044b2ad38",
"name": "pressure",
"description": "Any Perssure Tag is sufficient here to make a point",
"dataType": "Double",
"unit": "psi",
"unitGroup": "",
"dataSourceType": "APM_TIMESERIES",
"mappingValueType": "TAGS",
"isVariablePort": false,
"isRequired": false,
"isDirty": false
},
{
"@type": "analyticInput",
"hashCode": 0,
"uri": "/ports/d18223cb-7056-4fa3-834a-f69a7ec114b4",
"name": "rpm",
"description": "Any rpm Tag is sufficient here to make a point",
"dataType": "Double",
"unit": "rpm",
"unitGroup": "",
"dataSourceType": "APM_TIMESERIES",
"mappingValueType": "TAGS",
"isVariablePort": false,
"isRequired": false,
"isDirty": false
}
],
"constants": [
{
"@type": "analyticConstant",
"hashCode": 0,
"uri": "/ports/053310ff-e7f9-4ddd-982f-53aff0a566d0",
"name": "threshold",
"description": "threshold",
"dataType": "Double",
"unit": "None",
"unitGroup": "",
"dataSourceType": "CONSTANT",
"mappingValueType": "CONSTANT",
"value": "10",
"isVariablePort": false,
"isRequired": false,
"isDirty": false
},
{
"@type": "analyticConstant",
"hashCode": 0,
"uri": "/ports/d41d9e08-89f5-44f0-a5f3-2fde9bd4acf8",
"name": "threshold_attribute",
"dataType": "Double",
"unit": "None",
"unitGroup": "",
"dataSourceType": "CONSTANT",
"mappingValueType": "ATTRIBUTES",
"value": "",
"isVariablePort": false,
"isRequired": false,
"isDirty": false
}
],
"outputs": [
{
"@type": "analyticOutput",
"hashCode": 0,
"uri": "/ports/0085d7a3-cde9-4afb-afca-0e9305f8c4ae",
"name": "mean",
"dataType": "Double",
"unit": "None",
"unitGroup": "",
"dataSourceType": "APM_TIMESERIES",
"mappingValueType": "TAGS",
"isVariablePort": false,
"isRequired": false,
"isDirty": false
},
{
"@type": "analyticOutput",
"hashCode": 0,
"uri": "/ports/071d9648-c9f6-4863-a7b6-f0aaf4905378",
"name": "deviation",
"description": "Deviation output for alert-2. 1 if above the expr is true and 0 if it's false.",
"dataType": "Double",
"unit": "None",
"unitGroup": "",
"dataSourceType": "APM_TIMESERIES",
"mappingValueType": "TAGS",
"isVariablePort": false,
"isRequired": false,
"isDirty": false
}
],
"outputEvents": [
{
"@type": "analyticOutputEvent",
"hashCode": 0,
"uri": "/ports/314820bb-bf69-4689-b7fa-02b0399483f3",
"name": "cafAutomationAlert",
"unit": "",
"unitGroup": "",
"dataSourceType": "APM_ALARM",
"mappingValueType": "APM_ALARM",
"isVariablePort": false,
"isRequired": false,
"isDirty": false
}
],
"models": [],
"hashCode": -1723771949,
"analyticTemplateType": "HierarchicalType",
"isDirty": true,
"isAggregateEnabled": false
},
"isCustomInputSupported": false,
"isCustomConstantSupported": false,
"isCustomOutputSupported": false,
"isReadOnly": false
}
Runtime | Multiple Version Support? | Instructions To Upload And Save A New Version |
---|---|---|
GEDCR | Yes | To save a new version of the analytic (.zip or .jar) file, upload a new file, enter the new Analytic Version number, and then enter the Analytic Version Update description. The latest version of the analytic artifact will be used to run all future deployments. Existing deployments continue to use the currently assigned version unless you explicitly redeploy them to run with the new version. |
SmartSignal | Yes | To save a new version of the analytic (.zip or .jar) file, upload a new file, enter the new Analytic Version number, and then enter the Analytic Version Update description. The latest version of the analytic artifact will be used to run all future deployments. Existing deployments continue to use the currently assigned version unless you explicitly redeploy them to run with the new version. |
Power Datafabric | Varies | Depends on the runtime definition and configuration. |
Supported Data Sources
Data Source | GEDCR | SmartSignal | Power Fabric |
---|---|---|---|
APM Time Series | Yes | Yes | Yes |
APM Asset Attributes | Yes | No | Yes |
Constant | Yes | Yes | Yes |
Blobstore | No | No | No |
Any | No | No | No |
Postgres | No | No | No |
Predix Timeseries | No | No | Yes |
Modify an Analytic Template
Use the modify functionality to modify existing Analytic Catalog entries.
About This Task
You cannot modify the runtime type for an existing analytic template in the catalog. You may be able to modify only some fields for the selected analytic depending on its runtime type. You can see values in disabled fields but cannot modify them. For some other runtimes, you can change the field values using the AnalyticDefinition.json file.
Make sure you check all existing deployments that use the analytics template before you modify it. If your modified artifact has analytic implementation that is significantly different from the previously uploaded artifact in the catalog, consider creating a new analytic to add to the catalog instead of updating the existing one.
Procedure
Results
Delete an Analytic Template
You can delete an analytic template in the analytic catalog.
About This Task
Before you delete an analytic template in the analytic catalog, make sure that it is not being used in orchestrations or deployments. Deleting an analytic deletes its deployments. This cannot be undone.
Procedure
Disable Analytic Template Export (GEDCR Runtime)
Before You Begin
About This Task
Procedure
- In the Applications menu, navigate to .
- In the Search pane, locate and select an analytics to access it.
- In the workspace of the Analytics Template page, a Export Access window appears, select Enable/Disable Export.