User Actions
About Asset Groups Based on Queries
The ability to create an Asset Group based on a query allows a user to apply an analysis to a dynamic group of assets for example, equipment, functional locations, RBI components, etc. When a user bases a new Asset Group on a query, the Asset Group is dynamic in that it is subject to change as assets change with respect to the parameters of the query.
Every time you access an Asset Group that is based on a query, the query is freshly run. For example, the day you create an Asset Group using a query, the query it is based on may populate it with 10 assets. If you were to access the same Asset Group a month later, the query would run afresh and may populate the Asset Group with more or fewer than 10, depending on the number of assets that will meet the parameters of the query the second time around.
- ENTY_KEY
- ENTY_ID
- FMLY_KEY
- MI_SITE_KEY
When you apply an analysis to an Asset Group that is based on a query, the Asset Group is no longer dynamic. Instead, the assets returned by the base query at the time when you apply the analysis are the exact assets for which that analysis will always apply.
You cannot use an Asset Group that is based on a query as a filter in a module overview page or dashboard where asset filtering is available. You must convert the dynamic Asset Group to a static group to use it as a filter.
Create an Asset Group
Procedure
Filter Assets
Procedure
Search for an Asset
Before You Begin
Procedure
Create a Static Asset Group from an Asset Group Based on a Query
Before You Begin
Before you can create a static Asset Group from an Asset Group based on a query, the system must contain an Asset Group that is based on a query.
.
, and then, in the text box, enter at least two characters. For more information, refer to the Search section of the documentation.